STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Message Queue usage

Posted on May 25, 2017 at 15:47Hello all,I have problems with Message Queue in CMSIS-RTOS. I have following codefor putting C structures onto the Message QueueBOOL put_program_chunk(main_controller_req_t req){main_controller_req_t *p_req;BOOL retval...

How to stop a circular DMA at end of buffer

Posted on May 24, 2017 at 18:59Hi,I'm using an STM32F446.I use the circular DMA feature with a DAC output to generate a sinus waveform.My sinus buffer has 32 values.What I would like to do is :- run the DMA for a 'large' amount of time- be able to s...

Kuikui by Associate III
  • 3072 Views
  • 3 replies
  • 0 kudos

USART3 Interrupt not being fired

Posted on May 24, 2017 at 14:37Hey guys,I'm using a serial terminal to communicate with USART3 on an STM32F1 via an FTDI USB-UART converter cable. I am successfully receiving data from USART3 in my serial terminal but when I try to send data to it t...

Resolved! Need details about STM32 I/Os

Posted on May 24, 2017 at 18:24For my design i am already using STM32F429BI--LQFP208 package, Now i am looking to replace this with STM32F777BI-LQFP208, both are pin compatible..Question: In the data sheet of STM32F777BI Its mentioned that GPIO'S=15...

0690X0000060761QAA.png 0690X0000060766QAA.png 0690X000006076FQAQ.png 0690X000006070dQAA.png

Generate USART Tx DMA using timer expire on backend without any CPU intervention like DAC with Timer?

Posted on May 25, 2017 at 08:47Hi,    Generally i do likeOption 1)unsigned char tmp;unsigned char *ptr='Hello World!';for(tmp=0;tmp<10;tmp++){   HAL_UART_Transmit(&huart1,ptr,strlen(ptr),100);   HAL_Delay(10); //10ms}Option 2)Start TIM2 ,which gener...

Hobbyist by Associate II
  • 815 Views
  • 0 replies
  • 0 kudos

STM32F407 + LwIP + FreeRTOS: ethernet fritz

Posted on May 25, 2017 at 08:24If CHECKSUM run by SOFTWARE ethernet fritz in some packets (spam).//#define CHECKSUM_BY_HARDWARE in lwipopts.hEthHandle.Init.ChecksumMode = ETH_CHECKSUM_BY_SOFTWARE; in ethernetif.cHow can i fix it?

pestov by Associate III
  • 888 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F3xx device driver / lib lack

Posted on May 23, 2017 at 18:02I dont know I must be wrong but I didn't find function call to change the dutycycle of a pwm so I wrote this and I added it to stm32F3xx_hal_tim.c/**  * @brief  Set the PWM DutyCycle.  * @param  htim: TIM handle  * @pa...

o gaste by Associate III
  • 1377 Views
  • 2 replies
  • 0 kudos

Resolved! OPAMP output: VDDA overconsumption

Posted on May 22, 2017 at 15:35The STM32L471 Errata document states that:  An overconsumption can appear on VDDA in the following conditions:• a voltage VPAD is applied on PA3 or PB0 with VDDA+ 50 mV < VPAD < VDDA + 600 mV ...Our application uses ...

Chris1 by Senior III
  • 2533 Views
  • 6 replies
  • 0 kudos

How to receive a lot of characters from USART???

Posted on May 22, 2017 at 14:13HI I want Receive characters from USART. I don't  know how much characters will be sentand the data that will be sent is too much. in interrupt mode i will receive amount interrupts and it is not good(for example 1000 ...

l90mehdi by Associate II
  • 1888 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.