STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C Bootloader Issue - STM32L071KB

Posted on March 31, 2017 at 15:06Hi,   I have a STM32L071KB Chip Inserted in a  STM32F031K6-Nucleo Development Board.   I am trying to Get into I2C Bootloader mode by Setting BOOT0 Pin to HIGH.   But When I Try to detect the I2C Slave Address (0x42)...

0690X00000603j3QAA.jpg 0690X00000602RcQAI.bmp
Kannan M by Associate
  • 1773 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 USB CDC problem

Posted on May 30, 2017 at 10:07 hi everybody I'm using stm32l151 and I want to use usb peripheral in cdc mode. I used stm32 cubeMx to generate the project. when I connect the boar to PC, I can see the VCP in device manager.however I can't s...

mh2 by Associate III
  • 1992 Views
  • 3 replies
  • 0 kudos

measure pulse width using both edge input capture mode

Posted on April 26, 2017 at 13:41Hi Everyone,I want to measure the pulse width of a square wave signal and thought about using input capture mode and enable interrupt on both edges (rising and falling) and then in the interrupt routine i will read t...

Raider E by Associate III
  • 4959 Views
  • 3 replies
  • 0 kudos

How do you update the firmware on the SPWF01SA?

Posted on May 26, 2017 at 23:36I tried a search for this question and I cannot find an answer. How do you update the firmware on the SPWF01SA? I need to know what pins need to be set in which direction. For instance, the http://www.st.com/content/cc...

How to use iwdg in stop mode with stm32l0xx?

Posted on January 19, 2017 at 14:32Hi, I have a problem with low power mode. I want to use the watchdog with the stm32l0xx.But when I go in stop mode, I can not disable or frooze the watchdog counter (only possible with l4 family).And in a perfect w...

STM32F746G-DISCO display panel choice and alternatives

Posted on January 16, 2017 at 18:53 I bought a STM32F746G-DISCO board and have decided that a board like it will fit the needs of my project. Are there any companies that make development boards with this MCU that can use a larger LCD display? The ...

ray23 by Associate II
  • 13013 Views
  • 30 replies
  • 0 kudos

Request for enhancement : Cube 4.21.0

Posted on May 30, 2017 at 19:11Eric,In the implementation that was included in 4.21 there was a couple of MISRA violations inserted.Unlike the assert_failed routine, _Error_Handler uses char* and int for parameters instead of uint8_t* and uint32_t.J...

SW UART

Posted on July 19, 2016 at 16:55Hello, I need a sw emulated uart. I am trying to use the sw emulation available here:http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-periphe...

xfinta by Associate
  • 1418 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.