2017-05-30 10:11 AM
Eric,
In the implementation that was included in 4.21 there was a couple of MISRA violations inserted.
Unlike the assert_failed routine, _Error_Handler uses char* and int for parameters instead of uint8_t* and uint32_t.
Just a head-up.
Also, the USER CODE BEGIN and USER CODE END comments have an incorrect function name.
Andrei
2017-05-30 1:49 PM
Hi
Chichak.Andrei
,Thank you for your reported issue.
I will forward your request internally to our CubeMx team.
Thanks
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.