STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

H3LIS200DL SPI Configuration & Read

Posted on June 12, 2017 at 00:54Hello:According to all the documentation I can find, I have configured the STM32F4 correctly to interface to the H3LIS200DL accelerometer. This is for use in SPI3 (AF6). Somehow, there's still something amiss. When I ...

Usart 2 does not work

Posted on June 11, 2017 at 20:31I am trying to use 2 usart in my program. When i am trying send_to_uart2('a'); nothing happens. In debug mode USART2->SR is always 0x000. Why?#include 'stm32f10x.h'#include 'stm32f10x_gpio.h'#include 'stm32f10x_rcc.h'...

anton23 by Associate II
  • 1793 Views
  • 3 replies
  • 0 kudos

STM32Cube FW_F4 V1.14.0 error on SW4STM32

Posted on December 28, 2016 at 18:42Hi All,Maybe something went wrong on the new FirmWare template, because it generates the make command without double quote around  __weak= and __packed= switches like this:arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb...

zamek42 by Associate II
  • 1867 Views
  • 4 replies
  • 0 kudos

CUBE MX CMSIS-RTOS Incompatibilities

Posted on August 21, 2015 at 18:01I'm just starting with cube MX and free KEIL toolchain for STM32M0, wich includes free ARM CMSIS RTOS, and I have to say that I'm a little disappointed so far with RTOS implementation in MX. The only OS support is f...

I2C HAL For Protocols With Length Specified in Data

Posted on January 15, 2016 at 15:25I need to read from a device with a variable length response, where the length of the following data is specified in the first byte received.  I don't see a way to accomplish this using the HAL, as it appears you n...

jon2 by Associate II
  • 1952 Views
  • 4 replies
  • 0 kudos

Resolved! I2C HAL_I2C_ERROR_AF is set and the 2nd byte is not transmitted.

Posted on February 05, 2017 at 08:44using CubeMX V4.18.0. and uV5,  stole parts from the '091 examplesI can see the ACK from the slave device, on the Oscilloscopebuttrying to send 0x68, 0x0E,0x00,0x00 as a packetit sends 1 byte the 0x68 and stops.wh...

T J by Lead
  • 1728 Views
  • 2 replies
  • 0 kudos

hall sensor in stm32f103

Posted on June 10, 2017 at 12:58HiI am using stm32f103 to drive a BLDC motor with hall sesnors, I have found that stm32f103 has hall sensor mode to detect the motor posostion. how can I use this capability of stm32?* I am newly learning stm32 tnx

HAL method to output timer overflow interrupt to a pin?

Posted on June 10, 2017 at 03:25I think I'm not understanding the terminology, or something. I want to generate an external interrupt at a pin, when timer 2 overflows. I can generate an interrupt with the timer/counter just fine, it's the output to ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.