2017-06-11 11:31 AM
I am trying to use 2 usart in my program. When i am trying send_to_uart2('a'); nothing happens. In debug mode USART2->SR is always 0x000. Why?
#include 'stm32f10x.h'
#include 'stm32f10x_gpio.h'#include 'stm32f10x_rcc.h'void Delay(void)
{ volatile uint32_t i; for (i = 0; i != 0x140000; i++) ;}void send_to_uart1(uint8_t data)
{ while (!(USART1->SR & USART_SR_TC)) ; USART1->DR = data;}void send_to_uart2(uint8_t data)
{ while (!(USART2->SR & USART_SR_TC)) ; USART2->DR = data;}uint8_t uart_data;
int main(void)
{ GPIO_InitTypeDef PORTA_init_struct;RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_USART1 | RCC_APB1Periph_USART2, ENABLE);
PORTA_init_struct.GPIO_Pin = GPIO_Pin_9; PORTA_init_struct.GPIO_Speed = GPIO_Speed_50MHz; PORTA_init_struct.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &PORTA_init_struct);PORTA_init_struct.GPIO_Pin = GPIO_Pin_10;
PORTA_init_struct.GPIO_Speed = GPIO_Speed_50MHz; PORTA_init_struct.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &PORTA_init_struct); PORTA_init_struct.GPIO_Pin = GPIO_Pin_2; PORTA_init_struct.GPIO_Speed = GPIO_Speed_50MHz; PORTA_init_struct.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOB, &PORTA_init_struct); PORTA_init_struct.GPIO_Pin = GPIO_Pin_3; PORTA_init_struct.GPIO_Speed = GPIO_Speed_50MHz; PORTA_init_struct.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &PORTA_init_struct);USART_InitTypeDef uart_struct1;
uart_struct1.USART_BaudRate = 9600; uart_struct1.USART_WordLength = USART_WordLength_8b; uart_struct1.USART_StopBits = USART_StopBits_1; uart_struct1.USART_Parity = USART_Parity_No; uart_struct1.USART_HardwareFlowControl = USART_HardwareFlowControl_None; uart_struct1.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART1, &uart_struct1); USART_Cmd(USART1, ENABLE); USART_InitTypeDef uart_struct2; uart_struct2.USART_BaudRate = 9600; uart_struct2.USART_WordLength = USART_WordLength_8b; uart_struct2.USART_StopBits = USART_StopBits_1; uart_struct2.USART_Parity = USART_Parity_No; uart_struct2.USART_HardwareFlowControl = USART_HardwareFlowControl_None; uart_struct2.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &uart_struct2); USART_Cmd(USART2, ENABLE);while (1) {
send_to_uart2('a'); Delay(); send_to_uart1('b'); Delay(); }}2017-06-11 11:48 AM
>>Why?
USART2 is on APB1, not APB2, enable the right clock
2017-06-11 2:20 PM
I chaged to
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);But it do not work. value USART2->DR do not change.
2017-06-11 3:33 PM
The question asked about USART2->SR, which presumably now isn't zero?
Reading USART2->DR shows the content of the Reception register, it isn't the same thing as the Transmission register you write too, it is not a memory cell.
Avoid sitting the debugger over the USART, it will alter its behaviour, reading the DR will clear bits in the SR
If you want to read the same data back in DR, then loop the TX and RX together externally.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.