STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F7xx_hal_tim_ex.c Bug report

Posted on June 14, 2017 at 05:44 Hi all, i generated the pwm related source code using CubeMX 4.21 but it dit not work. Target MCU : ST32F746NG The following general PWM code works normally but not with DMA Functions. HAL_TIM_PWM_Star...

problem with startup on stm32f407

Posted on June 13, 2017 at 14:46very weird problem ive got here. im working on a big project which was passed over to me , so im quite new in this field and still studying the project as well. the programs runs, with no problems. i added a function ...

Do I need to lock interrupt on stm32?

Posted on June 14, 2017 at 11:28Hello,I wondered it writing / reading 32 bit values on a stm32 controller is atomic. The actual question is:If I have an interrupt handler which writes a uint32_t value and an application which reads the same value, d...

In burst mode, can addresses be increased?

Posted on June 14, 2017 at 10:47In burst mode, when the destination address is set to fixed, STM32F7 chip can increase the address? Because i see the Samsung chip can do this:So want to confirm the above content, thanks.#stm32f7-dma-brust

0690X00000603fvQAA.jpg
Eastar L by Associate
  • 682 Views
  • 0 replies
  • 0 kudos

FSMC_CLK is not running for muxed NOR configuration

Posted on June 05, 2017 at 08:27Hi,I am trying to configure STM32F207ZG nucleo board for synchronous muxed NOR flash and have configured for the same over cubeMX after generating the code i am calling HAL_NOR_Program and HAL_NOR_ReadBuffer in my cod...

0690X00000607EOQAY.png 0690X00000607EUQAY.png

Looking for documentation on moving ST Micro supplied SMT32F401RE example code over to the Nucleo STMF429zi

Posted on June 14, 2017 at 03:03Hello, I realize this is a basic question, but I am looking for documentation on how to move a ST supplied example (Specifically the X-CUBE-SPN2, X-Nucleo-IHM02A motor driver example) to the Nucleo STM32F429zi. The su...

How can I read data thru a GPIO configuread as EXTI?

Posted on June 13, 2017 at 12:32I'm trying to read an external ADC output.The data are provided thru a DRDY pin.When the DRDY falls, it generates an interruption in my STM32L1 (falling edge). Then, I must read the DRDY level eevery rising edge of a ...

amelendez by Associate III
  • 2088 Views
  • 6 replies
  • 0 kudos

STM32F7 Disco ADC issue

Posted on June 13, 2017 at 08:09Hello all,I am trying to read the ADC value from PA0 pin on a STM32F7 Disco board but without any success.The issue is that the ADC reading is acting as the pin is floatingI suspect that the initialization code is not...

STM32F412G-DISCO - how to configure FSMC using CubeMX

Posted on June 08, 2017 at 21:17Hi,I am big fan of the Discovery boards and whenever I buy a new one I try to configure it using CubeMX.As you know the provided examples are NOT generated by the CubeMX and there is no CobeMX project files available....

0690X00000602UnQAI.bmp
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.