STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Setup Custom HID device

Posted on February 27, 2017 at 23:01Hey guys.I'm trying to setup Custom HID. I'd like to use an output- and input Buffer.I have managed to setup the descriptors. I think i have done that right: Windows is correct enumerating my device.On the other s...

Check under debug mode for ARM semihosting

Posted on June 15, 2017 at 18:22I'm study cortex-m4 for semihost and use stm32f429-discovery board. I have a trouble with that semihost can not work when board is standalone(without in debug mode), So, I hope to use judge debug status before printf(...

ctc.ctc by Associate II
  • 1566 Views
  • 1 replies
  • 0 kudos

CooCox error while downloading code to STM32F103C8T6

Posted on August 29, 2016 at 16:09 Dear forum, i get this error after i tried to download the code to this board: http://artofcircuits.com/wp-content/uploads/2015/07/STM32F103C8T6-Development-Board-1.jpg I use a ST-Link V2 with ...

loder by Associate II
  • 3031 Views
  • 5 replies
  • 0 kudos

Cancel a pending UART recieve

Posted on January 16, 2017 at 23:02If i start an UART receive with an interrupt looking for the next inbound byte/char;HAL_UART_Receive_IT(&huart1, &UART1_Data, 1);how can i cancel the receive before receiving the next byte/char?

How to pass a variable read in an interruption to main()

Posted on June 14, 2017 at 15:14I'm reading a serial ADC from an interruption (24 bits)I need to pass its read value to the main()I have defined in /* USER CODE BEGIN PV */ a volatile variable uint32_t  xxxxxThe xxxxx variable is right inside the in...

amelendez by Associate III
  • 5464 Views
  • 12 replies
  • 1 kudos

RBUS issue on STM32F407

Posted on June 15, 2017 at 08:40Hello.I'm working on a new board with STM32F407 MCU.Currently, there's an issue with Ethernet.After board reset, Ethernet communication is working well.But after some time (minutes or hours), the Ethernet seems to be ...

Ho Lim by Associate II
  • 2032 Views
  • 2 replies
  • 0 kudos

STM32 F7 HAL CAN bug

Posted on March 21, 2017 at 15:31We are using HAL CAN drivers for STM32 F7 (stm32f7xx_hal_can.c).During CAN tx/rx stress tests we experienced an issue resulting in CAN receive hang.The issue is due to a race condition on hcan->State variable between...

STM32F103RBT6 Error: No device found on target.

Posted on June 05, 2017 at 11:24Hello, I've designed a custom board using STM32F103RBT6. To debug the custom board I've got the STM32F103 Nucleo-64 board. As mentioned in the User manual of Nucleo 64 board(UM1724) page 18, section 6.2.4, I've connec...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.