STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet reception - STM32F437

Posted on June 23, 2017 at 23:37We used to have a simple PHY attached to the MII port and it seems the less you did to configure it the better. Now we have replaced it with a Marvell 10 port switch. Two of the ports have no phy and are setup to talk...

John Hite by Associate III
  • 822 Views
  • 0 replies
  • 0 kudos

STM32L471 WFI problem

Posted on June 20, 2017 at 17:43On STM32L471 (DEV_ID=0x6415, REV_ID=0x1007)~4% of mcus do not enter standbymode and ignore the WFI instruction.Does anyone have ideas how to get it working on all mcus? (tested with 150 pieces)Is there any known bug/p...

damh by Associate II
  • 1785 Views
  • 3 replies
  • 0 kudos

Backup SRAM write failure (STM32F446)

Posted on June 22, 2017 at 07:20Hello.I have an issue using the backup SRAM on a STM32F446.The backup SRAM is used to store calibration data  which must be retained in case of a power fail reset. For that I connected the VBAT pin to a capacitor whic...

Resolved! [STM32F746-Discovery] Is it OK to use analog pins for UART7?

Posted on June 23, 2017 at 13:34Hello. I'm having problem with USART6 (again). So I'm testing now UART7. By checking documentation I have found that it is theoretically possible to set up uart7 on analog pins. I have made such conclusion after looki...

Ivan Ivan by Associate II
  • 1169 Views
  • 1 replies
  • 0 kudos

STM32F103C8 DSP Library problem

Posted on June 19, 2017 at 12:02Hello thereCan I compile the DSP library with STM32F103C8 device. I would like to import FFT using DSP library with this chip. But I get many errors when I compile the library.compiling main.c....\Library\DSP Library\...

Resolved! STM32L4 FMC Latched SRAM

Posted on June 09, 2017 at 08:41Hi All,I am currently working on migrating a system from a EFM32 ARM Cortex-M3 to the STM32L476VGT ARM Cortex-M4. In the current hardware implementation, the processor is connected to asynchronous SRAM via an FPGA  th...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.