cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32F746-Discovery] Is it OK to use analog pins for UART7?

Ivan Ivan
Associate II
Posted on June 23, 2017 at 13:34

Hello. I'm having problem with USART6 (again). So I'm testing now UART7. By checking documentation I have found that it is theoretically possible to set up uart7 on analog pins. I have made such conclusion after looking at p.21 of Discovery User Manual and by looking of p.76 of MCU User Manual:

MCU PINDISCOVERY CONTACT

PF10 : GPIO candidate (useful!)A1

PF9 : UART7CTSA2

PF8 : UART7RTSA3

PF7 : UART7TXA4

PF6 : UART7RXA5

I'm confused because contacts A1-A5 are marked as analog and they are hooked to Alternative Functions related to Analog-to-Digital-Converter (in Discovery User Manual). (I'm new with electronics and I'm afraid to damage the Board)

UART7 requires digital signals, I suppose.

Is it OK to use these Discovery contacts for UART7?

#stm32f746-discovery #uart #usart6
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
S.Ma
Principal
Posted on June 23, 2017 at 13:45

In microcontrollers, an 'analog pin' means Digital IO pin with additional analog capability (usually ADC analog to digital converter), so yes, these pins can be used for UART.

View solution in original post

1 REPLY 1
S.Ma
Principal
Posted on June 23, 2017 at 13:45

In microcontrollers, an 'analog pin' means Digital IO pin with additional analog capability (usually ADC analog to digital converter), so yes, these pins can be used for UART.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.