2017-06-20 8:43 AM
On STM32L471 (DEV_ID=0x6415, REV_ID=0x1007)
~4% of mcus do not enter standbymode and ignore the WFI instruction.
Does anyone have ideas how to get it working on all mcus? (tested with 150 pieces)
Is there any known bug/problem?
2017-06-20 9:37 AM
Are you looping on the WFI instruction? Anything driving NRST?
2017-06-20 12:05 PM
yes, it's the cube function [HAL_PWR_EnterSTANDBYMode()]
NRST has an external pullup (10k) and capacitor (100nF) to GND.
In one case NRST is connected additionally to the debugger or in second case open, but there is no difference.
All other units (144 pcs.) work correctly with the same firmware.
2017-06-23 8:05 AM
Is there a way to determine, why the wfi command is ignored? What flags have to be checked?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.