STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F07X using DMA transmit UART fail

Posted on August 01, 2017 at 04:08First, I introduce the background simply. I have program the STM32F072RB for somedays. I do this project start with STM32CubeMX. It�s going well until now. I have using the 2 DMA for SPI transmit before. And I want ...

0690X00000607mBQAQ.png
AMP HF by Associate II
  • 3674 Views
  • 7 replies
  • 0 kudos

Sine wave stability

Posted on July 10, 2017 at 07:49HelloI want to generate a 50Hz stable sine wave which I will amplify in order to obtain AC and DC voltage and current.The strategy is to generate the sine wave using DAC or PWM. I used one STM32 MCU with two DAC outpu...

ionutF by Associate III
  • 8414 Views
  • 17 replies
  • 0 kudos

usb cub mx

Posted on August 01, 2017 at 11:55HION STM32f cubmx mass storage device i need understanding device connect to pc or not please help me how can write program for understand cable is connect or not 

Resolved! Failed to erase an STM32F779NIH6 MCU

Posted on July 19, 2017 at 16:05Hello everybody,I have some trouble when I want to erase my chip by  sector erase  or mass erase (ST LINK UTILITY with ST LINK dongle)   I obtain  some  dummy bytes after an erase operation like that :00 00 00 00 00 0...

Julien M by Associate II
  • 2052 Views
  • 4 replies
  • 0 kudos

Resolved! STM32 with 3 12-bit analog watchdogs?

Posted on August 01, 2017 at 10:32Hello,I am searching for an STM32 device which offers 3 full 12-bit analog watchdogs.I have spent hours navigating on st.com but all I have found was the STMF303 line with 1x 12-bit watchdog + 2x 8-bit watchdogs.Can...

Resolved! Input capture Porblem

Posted on July 31, 2017 at 13:55Hey I use stm32f030p4 and i want counting a external frequency (Learning remote ).I configure timer  and interrupts like thisTIM_ICInitStructure.TIM_Channel = TIM_Channel_1;TIM_ICInitStructure.TIM_ICPolarity = TIM_ICP...

Resolved! CubeMX timing

Posted on June 07, 2017 at 20:18 Hi guys, I am running into some timing issue using CubeMX, probably after upgrading to the latest version. A couple of weeks ago I noticed my SysTick running roughly twice as fast as expected (half of 1ms) so I ch...

0690X00000607G5QAI.png
e d by Associate II
  • 7845 Views
  • 20 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.