2017-07-19 7:05 AM
Hello everybody,
I have some trouble when I want to erase my chip by sector erase or mass erase (ST LINK UTILITY with ST LINK dongle) I obtain some dummy bytes after an erase operation like that :
00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF 00 00 00 00 00 00 00 00 3C 29 00 08 29 21 00 00 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF BD 3B 00 08 BD 3B 00 08 00 00 00 00 BD 3B 00 08 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF BD 3B 00 08 BD 3B 00 08 00 00 00 00 BD 3B 00 08 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF BD 3B 00 08 BD 3B 00 08 18 08 00 00 BD 3B 00 08 FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF FF
Can I forget something ?
Normaly is filled by 0xFF ?
When I use this method on a STM32F103 it works well.
Of course when I try to put a firmware it become like a random firmware because the flash was not really erased.
Do you have some idea to help me ?
Thank you so much .
Julien.
Solved! Go to Solution.
2017-07-20 11:09 AM
Hi Julien,
Check all of our Hardware connections on board, including VDDs, VDDAs, VCAP Pins etc.. PDR_ON etc..
you can monitor VCAP pins with a voltmeter and check the value of ~1.2Volts. Hope it helps you.
Cheers,
STOne-32.
2017-07-20 11:09 AM
Hi Julien,
Check all of our Hardware connections on board, including VDDs, VDDAs, VCAP Pins etc.. PDR_ON etc..
you can monitor VCAP pins with a voltmeter and check the value of ~1.2Volts. Hope it helps you.
Cheers,
STOne-32.
2017-07-21 3:24 AM
Hi ,
Thank you so much for your help, my power path management seems to be wrong in my custom board , but in another one it works fine. thank you so much.
2017-07-21 8:12 AM
Hi,
Thank you but I try to test my other custom board (same batch) and I have some trouble STLINK tool can't erase all the time the board, if I use OpenOCD tools, I can erase sometime but with different time for sector 1 sometime 1 second and sometime 17 seconds and of course when I read again all byte stay in place. (erase failed) . I am so confuse, it is seems to be work but not always. Power issue on my schematic ? But 3.3V not so bad and 1.2V seems to be ok . 1 mistake maybe VCAP are 4.7uF and not 2.2uF do you think than it can be the cause of my issue ?
And when I succeed to flash correctly, the CPU won't start correctly just 1 time...
Thank you so much for your help.
Thank you community.
2017-08-01 3:11 AM
Finally, I found the issue, the power wires were not properly connected.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.