STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Advanced Timer to ADC trigger

Posted on August 16, 2017 at 18:56How can I trigger ADCs for injected conversion at CTR=PRD when my TIM8 is configured for up-down counting? I don't see any mechanism that can do this.

Framebuffer for STemWin Application in internal RAM

Posted on August 15, 2017 at 12:15I want to build my own hardware with a stm32f769 (with 512 kBytes internal RAM)I want to use the STemWin. The example 'STemWin_HelloWorld' supplied with the STM32F769I_EVAL Kit uses the external SDRAM.Due to cost sa...

Resolved! STM32F767ZI QUAD SPI

Posted on August 15, 2017 at 11:06Hello. I work with stm32f767ZI nucleo-144, and try use QUAD SPI bank1 to access W25Q128BV. All OK when i use 1 wire or 2 wire(dual mode), but when i use quad mode(4-wire), something went wrong. SPI Pins:            ...

Resolved! High values on unconnected GPIO pins

Posted on August 16, 2017 at 12:31 Hello. I'm developing an application based on Discovery board with stm32f429I. And now I have quite a weird issue:a high signal level is shown on unconnected input pins. Here is a code: //Configure PC4 ...

Ivan Ivan by Associate II
  • 2095 Views
  • 3 replies
  • 0 kudos

Resolved! Configuration of DMA for USART-RX buffer

Posted on August 14, 2017 at 17:23Hey there!I'm working on stm32f051 MCU for a little project and a I  have to receive and process data from its USART port 1.My issu is that I don't have any interuption from the DMA, and if I check directly on the b...

Sector Codes Can Bootloader

Posted on August 15, 2017 at 18:00According to AN3154 Datasheet I must write sector code in data field.But I dont know what is sector code and How can i find it for stm32f4 discovery?Just I want to erase sector by sector what I must do?(I know I mus...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.