2017-08-15 2:06 AM
Hello. I work with stm32f767ZI nucleo-144, and try use QUAD SPI bank1 to access W25Q128BV. All OK when i use 1 wire or 2 wire(dual mode), but when i use quad mode(4-wire), something went wrong.
SPI Pins:
PE2 ------> QUADSPI_BK1_IO2
PB2 ------> QUADSPI_CLK PD11 ------> QUADSPI_BK1_IO0 PD12 ------> QUADSPI_BK1_IO1 PD13 ------> QUADSPI_BK1_IO3 and i checked PF6 PB6 ------> QUADSPI_BK1_NCSAll wires work except PD13(PF6).
I Use Instruction - 1 Wire(0x94)
Address - 4 wire(24 bit all zeros)
Alt Bytes - 4 wire (8 bit 0xFF)
Dummy Cycle - 4 times
Data - 4 wire(wait for 2 byte)
Maybe I missed something.
I will be grateful for the ideas.
Sorry for English
.>:(
-------------------------------------------------------------------------------------------------------------------------
OK, i check errata sheet
(2.12.1 ), then i replaced dummy phase by alt bytes:Instruction - 1 Wire(0x94)
Address - 4 wire(24 bit all zeros)
Alt Bytes - 4 wire (24 bit 0xFF0000)
Data - 4 wire(wait for 2 byte)
But n
othing happens
, i attach new image, because something change on BK1_IO3.And i attached code where i use HAL to access QUAD SPI.
#stm32f767zi #quad-spi #w25q #bk1_io3Solved! Go to Solution.
2017-08-16 2:04 AM
The transfer of control commands beyond the first hardware access to memory - looks the same as in the documentation, but with a slight change. The low byte is transmitted / read first, just like all data.
Reading registers of external memory can give a faulty answer (at first glance), but it is serviceable - just not in the right order. We want to see how in the documentation x0.x1.x2.x3 We get x3.x2.x1.x0 - one big word in 32 bits.There is no coincidence with the documentation, the number of cycles is equal to the command + address. The reading of the data was omitted.
________________ Attachments : 25q64.h.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyGo&d=%2Fa%2F0X0000000b8g%2F0sBgOyo0Hh71Yhhrtdm.PYZV8y1QMYLoBrOvxW0_.Cc&asPdf=false2017-08-15 7:51 AM
The image does not match the documentation.
https://community.st.com/external-link.jspa?url=http%3A%2F%2Fnice.kaze.com%2FW25Q128BV.pdf
7.2.33 Read Manufacturer / Device ID Quad I/O (94h)2017-08-16 2:02 AM
Could you check out the new images and tell me where the discrepancy is?
2017-08-16 2:04 AM
The transfer of control commands beyond the first hardware access to memory - looks the same as in the documentation, but with a slight change. The low byte is transmitted / read first, just like all data.
Reading registers of external memory can give a faulty answer (at first glance), but it is serviceable - just not in the right order. We want to see how in the documentation x0.x1.x2.x3 We get x3.x2.x1.x0 - one big word in 32 bits.There is no coincidence with the documentation, the number of cycles is equal to the command + address. The reading of the data was omitted.
________________ Attachments : 25q64.h.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyGo&d=%2Fa%2F0X0000000b8g%2F0sBgOyo0Hh71Yhhrtdm.PYZV8y1QMYLoBrOvxW0_.Cc&asPdf=false2017-08-16 8:27 AM
I just made a record in the status registers, like you have in the attached file and the 0x94 command worked, thanks.
Later I noticed that in the documentation for SPI flash this is reflected in the paragraph '6.1.3 Quad SPI Instructions' at the bottom.
For today, reading ID is all I needed, thanks for help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.