cancel
Showing results for 
Search instead for 
Did you mean: 

ADC1&3 w/ext trig, bad code from CubeMX w/NucleoF303ZE

Larry Lukis
Associate II
Posted on March 27, 2017 at 14:15

Start with new CubeMX project, selecting NucleoF303ZE board. Enable 1 single ended channel on each of ADC1 and ADC3. Select Regular Conversion Trigger for both. 

CubeMX generates this line in MX_ADC3_Init():

  hadc3.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_EXT_IT11;   // incorrect

IT_11 is incorrect for ADC3, it should be EXT_IT2

  hadc3.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_EXT_IT2;   // correct

.ioc file attached.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Imen.D
ST Employee
Posted on March 27, 2017 at 15:53

Hi,

Which CubeMx version are you using ? I will check this case then come back to you.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on March 27, 2017 at 16:17

4.20.0

Thanks,

Larry

Posted on March 29, 2017 at 18:01

Thank you Larry for your reported issue. I raised this error internally to our CubeMx team.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Sirma Siang
ST Employee
Posted on August 24, 2017 at 15:46

Hello

Lukis.Larry

,

I would like to thank you for your feedback.

I confirm you that the correction will be in CubeMX 4.

Kind regards

Sirma

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.