STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LQFP-64 thermal resistance Rjc

Posted on September 07, 2017 at 17:52Hello,i would like to know what is the thermal resistance Rjc for a package LQFP-64. I didn't saw the value in the datasheet and i need it to know the Tj temperature, when PDmax is 0.1mW and my case is 90degrees....

STM32F429 Interrupt question.

Posted on September 07, 2017 at 17:01Hi I've made an interrupt example with referring ST's EXTI_Example.The code is below, and it seems working, but I'm not sure it works whether correct.Because, I've expected that the PG14 LED will keep running whe...

[OTG + documentation] split sentence

Posted on August 25, 2017 at 23:43More.Thisis one sentence - The core reserves this space in the receive data FIFO to write SETUP data only, and never uses this space for data packets.Seen across all OTG chapters in all checked RMs.JW

0690X000006081GQAQ.png

Bug in STM32CubeMX v 4.22.0 with dual ADC mode

Posted on July 11, 2017 at 18:48When I had generated code with dual ADC on regular simultaneous mode from STM32CubeMX, the code after compiled couldn't get to work and rised error handler, so I traced the problem, found that there is a multiple mode...

0690X00000603wIQAQ.jpg 0690X00000603szQAA.jpg 0690X00000603t0QAA.jpg 0690X00000603wMQAQ.jpg

Resolved! What is hardfault?

Posted on September 07, 2017 at 18:02I want to know more about hardfault.1-)Is there any documentations about hardfault on stm32f415 microprocessor?2-)Why does Hardfault occur(all reason)?3-)Are there any difference between the processors(for exampl...

four uarts on stm32L433?

Posted on September 05, 2017 at 22:05Is it possible to get four USART/UART devices at once on the STM32L433 in a 64-pin package? I need one UART for input, one for output, one for external logging, and USART1 for debugging.Is this doable? I've used ...

Square wave generation with STM32 and timer

Posted on September 06, 2017 at 22:27hi everyone,I'm trying to generate a square wave / quadrature signal ( 2 square wave with 90 degrees offset). The board is a STM32F103C8The goal of the project will be to send an exact number of pulse. Frequency ...

paul sauv by Associate III
  • 1854 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.