STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

conflicting SPI3 and remapping macros

Posted on September 10, 2017 at 12:08in my embedded system there is an stm32f103vdt, working with spi3 and usart3(remapped). spi3 is working well and the problem occurs when i configure usart3 remapped. as i call the macro __HAL_AFIO_REMAP_USART3_EN...

How can I use the alternate function mapping?

Posted on September 11, 2017 at 06:17Hi.Now I'm trying to understand the alternate function mapping with simple example of  'STM32F4xx_StdPeriph_Examples\USART\USART_HyperTerminal'But there is nowhere the setting of alternate function mapping to use...

Generate Timer 3 Interrupt every 2 seconds

Posted on September 11, 2017 at 09:12Greetings,I want to generate timer3 interrupt every 2 seconds.  Below is my timer3 init code. I am using CUBE MXstatic void MX_TIM3_Init(void){TIM_ClockConfigTypeDef sClockSourceConfig; TIM_MasterConfigTypeDef sM...

Resolved! Event Recorder on STM32F030K6t6 error

Posted on September 10, 2017 at 11:01 hi i haveSTM32F030K6t6 that have 4KB Ram when i try to use Event Recorder on keilit get me this error *** Using Compiler 'V5.06 update 4 (build 422)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin' Build target 'Ta...

STM32F437 exiting standby incorrectly

Posted on November 02, 2015 at 10:56 Hi there, I'm currently having some issues with the STM32F437 package going into standby, whenever I send the instruction to go into standby the device goes to sleep but then almost immediately wakes b...

Which pin should I have to use to test USART1?

Posted on September 09, 2017 at 16:52Hi.I'd like to test UART in STM32F429-DISCO kit, and I buy UART to USB board But I don't know what pins are using in UART test with .STM32F4xx_DSP_StdPeriph_Lib_V1.8.0Could you please let me know which pins shoul...

0690X000006046CQAQ.jpg 0690X00000608BVQAY.png

EEPROM emulation

Posted on September 11, 2017 at 06:31Hello I use stm32f030 with 16K flash.i want save 22 byte with EEPROM emulation  and use keil.my program use 15720 byte of flashProgram Size: Code=15720 RO-data=212 RW-data=200 ZI-data=2856 i use this option and a...

Jlink could not halt CPU during linking STM32F103VET6

Posted on September 09, 2017 at 04:35Hello,I have a trouble using STM32F103VET6.I attached the reset and boot circuitary.i have assembled three boards and tested.Unfortunately, one of them was normal, but the others were not.The trouble is as follow...

KUHAN JON by Associate II
  • 3116 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.