2017-09-11 3:47 AM
Part number is STM32F303CC.
A 24 MHz oscillator output is connected to PF0 pin.Exiting from reset (either via nRST pin or SCB_AIRCR SYSRESETREQ bit), and having BOOT0 pulled up and USB cable connected, the bootloader waits forever for RCC_CR HSERDY bit to become 1.
The same identical problem presents with BOOT0 low, thus starting from Flash and jumping to the internal bootloader (SP@0x1FFFD800 and Reset@0x1FFFD804) - that is what we want to do.BUT If I power cycle the board, everything works as expected (USB DFU bootloader up and running).
Is the bootloader supposed to start following a reset (as it is described on the refman and as it happens on other parts we have worked with)?
Am I missing something?Solved! Go to Solution.
2017-09-11 4:16 AM
>>The same identical problem presents with BOOT0 low, thus starting from Flash and jumping to the internal bootloader (SP@0x1FFFD800 and Reset@0x1FFFD804) - that is what we want to do.
Do you map the ROM so that is shadows into the zero address space? SYSCFG mapping register
2017-09-11 4:16 AM
>>The same identical problem presents with BOOT0 low, thus starting from Flash and jumping to the internal bootloader (SP@0x1FFFD800 and Reset@0x1FFFD804) - that is what we want to do.
Do you map the ROM so that is shadows into the zero address space? SYSCFG mapping register
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.