STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STemWin problem: EDIT text bug

Posted on September 25, 2017 at 21:42I've got a bug with the text of the Edit box. It show's strange chars or drawings, maybe another language font. I'm using the emwin with the SSD2119 driver. All other fixed texts and labels are correct (see the a...

STM32L4 USB VCP Receive Buffer Issue

Posted on September 25, 2017 at 19:41Hi,I am using STM32L4 Discovery board, I have generated USB VCP code from cube MX and configured as CDC class in Device mode. I am facing an issue with Receive buffer, I don't understand the issue. If host send d...

Sunny T by Associate
  • 1576 Views
  • 2 replies
  • 0 kudos

A suggestion for a new register in STM32 processors

Posted on September 25, 2017 at 20:17When using watchdog timers, the processor resets when your program fails to clear the watchdog timer within a predetermined period. The RCC_CSR has two bits that can be queried at boot time that indicate a watchd...

gdb client exectuable path for Segger JLink

Posted on September 25, 2017 at 19:28Hi all,I'am working on a project with System Workbench for STM32.Does anyone of you know what the absolute path is for the gdb client executable, when using Segger JLink debug /programming adapter? Where can I fi...

Max Veen by Associate II
  • 659 Views
  • 0 replies
  • 0 kudos

STM32 DFSDM - simultaneous sampling of multiple channels

Posted on September 25, 2017 at 15:11I am a bit confused about the capabilities of the STM32 DFSDM module. The documentation says (section 17.3.77) that the channels selected for are converted one after another, but is it possible to sample multiple...

quad SPI to SPI DMA

Posted on September 24, 2017 at 12:31Hello,I have a data in stored in quad SPI memory on device A, that I want to transmit to device B using SPI interface.I was wondering if its possible to steam directly from quad-spi memory to SPI interface using ...

priven by Associate II
  • 1276 Views
  • 2 replies
  • 0 kudos

Unable to debug STM32F100 discovery with STM32_SW4

Posted on September 25, 2017 at 15:10Hi,    I am daily using STM32_SW4 to debug STM32F4 and STM32F4 boards. Now I am trying to do some debug on a STM32F100 discovery board but the debugger does not connect. The jumper on CN3 are set. I can connect t...

raffin by Associate III
  • 831 Views
  • 0 replies
  • 1 kudos

DMA + FATFS + RTOS

Posted on September 25, 2017 at 15:08Hi I start project with cubemx 4.17. I want to use DMA + FATFS + RTOS. Cubemx 4.17 not support this option. I migrate to cubemx 4.20.  Then i generate project for truestudio and run on board. Board not work and u...

bar Boss by Associate
  • 656 Views
  • 0 replies
  • 0 kudos

Resolved! What am I supposed to do to use PA14, PA15 in STM32F103xx?

Posted on September 25, 2017 at 10:45Hi.In the STM32F103, I'd like to control PA14, PA15 pin to I/O, But It's not controlling as my mind.When I checked that with reference document, I found the below information.I think If I want to use PA14 and PA1...

0690X00000608M0QAI.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.