STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f4 Usb VCP corrupted data (CubeMX)

Posted on September 22, 2017 at 19:01Hi,I have a problem while implementing a USB Virtual Com Port (USB CDC Class) with CubeMX.The setup is the following:PC running Hyper Terminal sends keystrokes to the microcontroller (STM32F407VG) which are echoe...

Timer output don't stop

Posted on September 26, 2017 at 12:09 I am doing a program where I have a 50Hz square signal and a PWM to generate a sinusoidal with 90 points. Each time the signal edge of 50Hz is raised or lowered, the timer must be reset and start a new mod...

0690X00000602UbQAI.bmp

Parallel read of GPIO using DMA for periph to mem

Posted on September 26, 2017 at 12:06Hey everyone,I need to read in my data using two GPIO's with an external clock.I've read a few docs including the AN4666 which seem to have gotten some form of this working.It seems like the DMA can be triggered ...

con3 by Senior
  • 812 Views
  • 0 replies
  • 0 kudos

STM32F091CCU6 Controller

Posted on September 26, 2017 at 07:54Hi All,I used 'STM32F091CCU6' this controller.Can I Implement OTA in this controller.  Please give me soluation as soon as possibleRegardsNitin Kanani#stm32f091 #stm32ff103 #stm32f091ccu6 #stm32f

STM32Cube does not run

Posted on September 25, 2017 at 22:10I just installed STM32CubeMX on my Windows 10 machine.  When I try and launch it, I get the following error.  How can I fix this?  I have Java installed- for many environments and the Java About returns the messa...

0690X00000608NIQAY.png 0690X00000608NlQAI.png
ttatakis by Associate III
  • 1275 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.