2017-09-25 6:10 AM
Hi,
I am daily using STM32_SW4 to debug STM32F4 and STM32F4 boards.
Now I am trying to do some debug on a STM32F100 discovery board but the debugger does not connect. The jumper on CN3 are set. I can connect to the board with the STlink utility v.24 and STLink v4.0. I can erase flash and I also upgraded the STLink firmware to the V1.J12.SO.
Why I can't debug the discovery using the ST32_SW4? The error I get is 'Unpluggeg target or STLINK already in use' but both statemens are false.
This the error detail:
Error in final launch sequence
Failed to execute MI command:-target-select remote localhost:3333Error message from debugger back end:
localhost:3333: Il sistema ha tentato di unire un'unità con una directory su un'unità unita.localhost:3333: Il sistema ha tentato di unire un'unità con una directory su un'unità unita.When I connect with the STLINK utility I get
15:01:13 : ST-LINK SN : ST-Link/V1_on_F:
15:01:13 : ST-LINK Firmware version : V1J13S015:01:13 : Connected via SWD.15:01:13 : Connection mode : Normal.15:01:13 : Debug in Low Power mode enabled.15:01:13 : Device ID:0x420 15:01:13 : Device flash Size : 128KBytes15:01:13 : Device family :STM32F100xx Low/Medium density Value LineThank you in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.