2017-06-01 4:59 AM
Hi,
I'm quite new to ST environment so please excuse any big mistake.
I,m using STM32CubeMX (4.20.1) and a Nucleo F429ZI to evaluate for an upcoming project. While experimenting with ADC I've realized that with Scan Conversion Mode enabled for 3 ADC channels (ADC1) the generated code doesn't configure the sampling time for the 2nd and 3rd channel.
Is this a bug or I'm doing something wrong?
Best regards,
static void MX_ADC1_Init(void)
{ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.ScanConvMode = ENABLE; hadc1.Init.ContinuousConvMode = DISABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 3; hadc1.Init.DMAContinuousRequests = DISABLE; hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_TEMPSENSOR; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_480CYCLES; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank = 2; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_VREFINT; sConfig.Rank = 3; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); }}
2017-09-26 4:21 AM
Hi,
sConfig variable sets its SamplingTime field to ADC_SAMPLETIME_480CYCLES at first, then this structure is used for next calls without change to this SamplingTime field.Did you check with debugger that the SamplingTime value field is passed to HAL_ADC_ConfigChannel() with the same value?
Regards.
Cyril
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.