STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Calling stm32429I-Eval Bootloader

Posted on May 02, 2014 at 01:26Hello, we are wanting to call the built-in bootloader from our application without manipulating the BOOT0/BOOT1 pins. I am trying to use the EVAL board to validate our method. The Users Manual for the Eval board does s...

chuck2 by Associate
  • 23557 Views
  • 32 replies
  • 2 kudos

Resolved! Does STM32L072 support USB programming/debugging?

Posted on October 04, 2017 at 07:37Hello All,Is it possible that STM32L072 can be programmed/debugged through USB?  It would be nice if somebody could share reference to the possible ways the micro-controller can be programmed/debugged.Best Regards,...

sarang2 by Associate
  • 1574 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L4 Demodulated Infrared Receiver Input

Posted on September 27, 2017 at 14:16Greetings community,I am developing an IR learning hardware that can transmit its learned IR codes as well. For the transmitter part, I will be using the IR_OUT pin (PA13).For the receiver part, from AN4834, I un...

STM32F030 was reconfigured by himself - help

Posted on October 03, 2017 at 13:32Hi community,I need help again. I have a problem with my stm32f030RCT6 program. Yesterday I programmed this MCU and today morning a saw problem. Problem is with reconfiguring rcc settings. MCU was programmed with P...

Arm-Gcc MakeFile Windows

Posted on October 04, 2017 at 11:55Simply I am trying to program my stm32f4 discovery without any ide.Another word I want to use  make command on the terminal in Windows.I know this makefile wrote for macos I cant convert the code working under  Win...

USB pull up USB_FS_DP line

Posted on February 03, 2017 at 09:31I use ''USB Device'' on STM.My STM32F401 has USB OTG so it means that it can pull up USB_FS_DP data line without pull up resistor .But I can't find a way how to do it, please help me

0690X00000606EDQAY.png

audio weaver startup problem on Windows 10

Posted on October 04, 2017 at 15:50I installed audio weaver ''Audio_Weaver_Designer_6.17.06_STMicro'' on Windows 10, 64 bit. I actually installed and uninstalled multiple times, thinking the installation failed.I get the following error on startup. ...

0690X00000608TtQAI.png

STM32F302RBT6 compatible with STM32F302R8T6

Posted on September 19, 2017 at 23:27Hi,We are using the device STM32F302R8T6 on our current design. Can I replace this part with STM32F302RBT6 without making firmware changes? I checked on datasheet and found STM32F302RBT6 has everything what STM32...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.