STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f373 sdadc switching configuration

Posted on October 04, 2017 at 13:01 Hello everyone! I'm working on the project with an STM32F373 microprocessor. I'm using all three SDADC-s simultaneously. SDADC3 works constantly in Injected scan mode with frequency 16,66kHz. SDADC1 and SD...

HAL_ERROR in HAL_RCC_OscConfig()

Posted on September 29, 2017 at 18:13Hi all!I have an STM32L0 using the HSI to clock at 6MHz, and a LSE for the RTC.Devices goes to sleep (STOP mode) and wakes up just fine.But if I activate the RTC Alarm A interrupt, while restoring clocks I get a ...

STM32F407Z and FatFS. Mounting SD Card issue.

Posted on October 04, 2017 at 10:50Simple problem description: f_mount function from FatFS causes stack problem somethere is parallel tasks in FreeRTOS.More detailed description:We have a project in which we use the processor STM32F407Z and we have ...

Oleg M by Associate
  • 756 Views
  • 0 replies
  • 0 kudos

STM32L4 TIM2 Configuration for Infrared Receiver

Posted on October 04, 2017 at 09:39Dear community,Below are my configuration to capture infrared signals from the TIM2 CH1. Can I get confirmation that I may use these configuration for my purpose;Best Regards,Mete#receiver #stm32l4 #pwm #tim2 #inpu...

0690X00000608T5QAI.png 0690X00000608TFQAY.png

DAC specification 8-10bit mode?

Posted on October 04, 2017 at 04:21STM32F4xx1: Do 8bit DAC mode have same specifications as the 10bit mode?2: The 3.3V / 1.5MOhm = 2.2 µA load for 1% accuracy as spec'ed in manual is for internal    buffer off , i had assumed no load at all would g...

Minimum input voltage for stm32f0

Posted on October 03, 2017 at 09:56Hello ST community,What if I provide 2.8V as a Vcc to STM32F0? Does it behave properly?Yes, I have checked input voltage range is 2.4V to 3.6V, still wanted to confirm with you because usually we provide 3.3V to su...

deokar by Associate II
  • 2538 Views
  • 3 replies
  • 0 kudos

Understanding interruptions

Posted on October 03, 2017 at 17:54Hi.I am currently working with a STM32L476 Discovery board.I just want to start an interruption handler with a basic timer, but I am facing an issue.I would like to toggle a LED from the board when the timer is res...

azer asd by Associate II
  • 1606 Views
  • 2 replies
  • 0 kudos

STM32F103 Loss RTC Date when RESET

Posted on August 30, 2017 at 11:18Hello friendsi using STM32CubeMX 4.2.2 & Firmware F103 v1.6 , MCU = STM32F103ZET6I set the time and date in RTC When micro resets I miss the date but time is still rightHow do I fix this problem?Thank,

Pedram by Associate III
  • 2917 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.