STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RD pin (FSMC_NOE) required?

Posted on October 12, 2017 at 15:02HiThere is no RD pin on the lcd.there are only WR, RS, CS and 16 bit data bus.RD pin (FSMC_NOE) required?  Thank you.void LCD_CtrlLinesConfig(void){ GPIO_InitTypeDef GPIO_InitStructure;/* Enable GPIOD, GPIOE, GPIOF...

kemal by Associate II
  • 1371 Views
  • 1 replies
  • 0 kudos

STM32F446 Offset two 3-Phase PWM-Signals

Posted on October 12, 2017 at 14:51Hi,I am trying to sync two three phase center aligned PWM signals on my STM32F446.Goal is to habe the center of the two PWM signals to be offset by half of the base frequency.Is this possbile and if yes how do I co...

STM32L476 Nucleo UART/HAL looses characters on TxD

Posted on October 12, 2017 at 10:04Hi,trying to transmit data via USART1 of STM32L476 Nucleo evaluation board. Use PA9 for TxD.Character count is 254*2+14 = 522  or   255*2+14 = 524.522 always is ok, 524 gives errors at receiver site.Data switches b...

JuM by Senior
  • 2384 Views
  • 5 replies
  • 0 kudos

HAL_SPI_TransmitReceive_DMA() missing error handling

Posted on October 12, 2017 at 16:30Not a question, but an observation. I am using the STM32L476G-EVAL board with STM32Cube_FW_L4_V1.9.0 and noted that within the call to HAL_SPI_TransmitReceive_DMA(), if calls to HAL_DMA_Start_IT() do not succeed fo...

STM32F4 system headers and OPTCR1

Posted on February 27, 2017 at 12:09Hello,even so e.g. OPTCR1 seems to to be used on STM32F401, system headers define values with OPTCR1. This pollutes the headers.

Stm32f4 discovery board:STLINK not connected

Posted on October 12, 2017 at 14:26Hello,I am using stm32f4 discovery board, but when I am trying to connect the board to pc I am gettingerror: 'One of the USB device connect to this system is malfunctioned'.In device manager error is ' Windows has ...

Resolved! problem with FLASH_OB_ProgramData stm 32

Posted on September 22, 2017 at 09:07HELLO I USE STM32F100RBI WANT write and read from flash mem :static HAL_StatusTypeDef FLASH_OB_ProgramData(uint32_t Address, uint8_t Data);static HAL_StatusTypeDef test3;/********************FLASH MEMORY*********...

please,To reduce internal RTC errors

Posted on October 11, 2017 at 04:32Hello, I am going to use the internal RTC. However, there are a lot of errors when using the internal RTC. I wonder if there is a way to reduce errors.I don't know because I'm a beginner. Thank you for giving me a ...

HG LEE by Associate II
  • 2547 Views
  • 5 replies
  • 0 kudos

STM32F4 USB VCP

Posted on October 11, 2017 at 13:27Hi guys,I'm using an STM32F446 micro-controller with USB CDC stack configured as VCP.Each time that i connect a device the operating system (Win 7) assign a new COM port number to the connected device.I know it's a...

Bucky by Associate II
  • 2056 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.