2017-10-12 5:26 AM
Hello,
I am using stm32f4 discovery board, but when I am trying to connect the board to pc I am getting
error: 'One of the USB device connect to this system is malfunctioned'.
In device manager error is ' Windows has stopped this device because it has reported problems. (Code 43)'.
and LD8 is also on.LD8:Red led indicates an overcurrent from the VBUS of CN5.
Is stm32f4discovery board damaged?
Thanks
Regards,
Mohit Rai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.