STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32l476v TIM15 CH2 PWM not working from cubeMx

Posted on October 16, 2017 at 09:37Hi, I'm trying to start a STM32L576VGT with FreeRTOS.I have a led blinking from a task and now I'm trying to set a PWM on, freq and duty is not important now, is a 'hello world pwm'.All is done using CubeMx, and I'...

SD Card for STM32F767ZI Nucleo Board

Posted on October 16, 2017 at 08:57Hello All,I wanted to use SD card (actually SDIO card) in STM32F767ZI Nucleo Board.Any suggestion for add-in available for SD card interface?Or Any Base Board/Daughter board to support SD card interface?Thanks!!reg...

Hardfault during SRAM Code execution

Posted on October 14, 2017 at 16:36Hello, I am using stm32f407 discovery board and when i tried to execute the code stored in the SRAM i am getting hardfault exception . the instructions are indeed valid. i have attached the screenshot which shows t...

0690X00000608c7QAA.png
n.serina by Associate III
  • 2322 Views
  • 6 replies
  • 0 kudos

Best way to combine reset signals for STM32

Posted on October 14, 2017 at 04:48Hi,I have a design that has two STM32s in it, for this application I would like them to be able to reset each other. On top of that, there would be the physical reset button and the SWD reset signal.What is the 'st...

Coratron by Associate II
  • 3436 Views
  • 3 replies
  • 0 kudos

STM32F405 No USB VCP generated from CubeMX

Posted on October 15, 2017 at 15:02Hello,I have a board with a Stm32F405, which is connected to my PC via USB.DFU flashing works well, but I cannot start a VCP Stack.I generated a project with STM32CubeMX, selected the FS-USB-Device and added CDC as...

0690X00000608cDQAQ.png

Why __HAL_TIM_CLEAR_IT at start of interrupt?

Posted on October 15, 2017 at 01:10HelloWhy does the HAL library call '__HAL_TIM_CLEAR_IT' before calling the 'HAL_TIM_PeriodElapsedCallback' callback, instead of after?I previously had a bit of code running before the 'HAL_TIM_IRQHandler(...)' in s...

Could you explain about 'Timeout' argument?

Posted on October 14, 2017 at 08:12Hello, I'm high school student(not good at English...), very interested in STM32 board. I'm studying about SPI using STMCubeMX, and I know there is HAL_SPI_Transmit function.But I couldn't understand about 'Timeout...

0690X00000608bYQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.