STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_Delay() function always last 1 ms more

Posted on October 19, 2017 at 14:11I'm using the latest build of CubeMX with a F429 Disco kit. If I use HAL_Delay(1) it last 2 ms, HAL_Delay(5) last 6 ms to get 1ms HAL_Delay(0) must be used.This is a major bug that should be fix ASAP!

sergetr by Associate II
  • 1415 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F405VG SDIO interface

Posted on October 19, 2017 at 13:55Hi community!I would like to connect STM32F405VG SDIO interface. What is the best way to do it?I implemented the following example:Best regards.

0690X00000608fuQAA.png

STM32F407 - USART6 Tx Frame Error

Posted on October 18, 2017 at 10:31Hi All,I tried to use USART6 but the data I sended is corrupted, I check the baudRate bur its looks fine(9600 bps), I add the screen shot of oscilloscope I send 0x79(0b0111 1001) but its showed me irrelevant data, ...

ygt_1108 by Associate II
  • 10999 Views
  • 19 replies
  • 0 kudos

How can I stop on PC=0 for debugging?

Posted on October 19, 2017 at 10:53I'm currently working with MDK and ULINK2 JTAG debugger in STM32F103C8.I want to stop Program Counter = 0; for debugging.But currently as much as I can stop debugging point is just PC = 0x80000178.Is there any way ...

0690X00000608gsQAA.png

Resolved! My stm32CubeMx can't open built-in datasheet.

Posted on October 16, 2017 at 02:56 When I installed the software for the first time, it works fine. Clicking 'Datasheet' icon will open the pdf file. Now this icon is shown as gray, and can't be clicked. I have downloaded all the documents on my...

ADC external-Trigger Options

Posted on October 11, 2017 at 14:34I am using the STM32F427 micro and a Keil compiler and have a question about external and timer trigger possibilities with the ADC. I have ADC1 and 2 configured for dual simultaneous mode and scanning through 12 co...

0690X000006048hQAA.jpg 0690X000006046mQAA.jpg 0690X000006048nQAA.jpg 0690X000006043eQAA.jpg

why led blink when any clock source not selected?

Posted on October 19, 2017 at 10:42hi,on this code:&sharpinclude 'stm32f10x.h'&sharpinclude 'delay.h'int main(){      SystemInit ();  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA , ENABLE);        GPIO_InitTypeDef gpio;  gpio.GPIO_Pin = GPIO_Pin_0;  ...

Resolved! QSPI usage in STM32F769NI disco board

Posted on June 30, 2017 at 14:57Hello Team,I have purchased STM32F7 disco board. I want to use CubeMx tool to generate code and modify/use it.Can I get CubeMx project for STM32F7 discovery board : STM32F769i - DISCO (MB1225B)Thank you,

Resolved! STM32L0 custom board does not connect below 3.0 V

Posted on October 18, 2017 at 19:42Hi all,My custom designed bare STM32L052C (QFP48) board refuses to talk to external debuggers (STLinkV2, JLink) when the power goes below 3.0 Volts on Vdd pins.Only SWD interface and step-down power source are conn...

Trouble with Power STM32L031K6

Posted on October 19, 2017 at 11:00Hello, I work with a microcontroller STM32L031K6 and as soon as it arrives at 3.3 V the battery falls from 3.3V to 2V and it is no longer functional. you have an idea. pleaseMy battery it's Lithium  LI-SOCL2 - 1750...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.