2017-10-19 5:11 AM
I'm using the latest build of CubeMX with a F429 Disco kit. If I use HAL_Delay(1) it last 2 ms, HAL_Delay(5) last 6 ms to get 1ms HAL_Delay(0) must be used.
This is a major bug that should be fix ASAP!
2017-10-19 6:01 AM
Don't rely on these routines for precision timing, the granularity is already poor, try a time base that clocks 10x the resolution you want. Consider using DWT_CYCCNT, that has ~5ns granularity, and might deliver +/-20ns accuracy.
>>
This is a major bug that should be fix ASAP!
No, you're using a function that's inappropriate for your application.
2017-10-19 6:27 AM
Loopdelays are usually meant as 'delay at least as much as the argument says'.
The documentation should clearly state this - did you check it?
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.