STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Having trouble with USART6 RECEIVE

Posted on October 19, 2017 at 20:57Hi, I am having trouble getting my USART6 receive on PORT PC7 working.I have USART6 initialized at 115200 baud in TX and RX mode and can transmit fine on USART6 PORT PC6. In order to test USART6 reception I have a ...

Icons and DMA2D / STM32F746

Posted on July 07, 2017 at 04:55Hi, I currently have STM32F746 connected to a 640x480LCD which is working as expected.I'm using one LTDC hardware layer and doing everything through DMA2D and an external SRAM. So far all is good, I can load images an...

S A by Associate II
  • 1542 Views
  • 2 replies
  • 0 kudos

Resolved! Timer16 PWM Not Working

Posted on October 20, 2017 at 02:46I am using an STM32F072B-DISCO. I am trying to get a PWM on pin A6 using timer 16. The timer seems to be counting as expected, but there is no output on A6.Here is my code:    RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GP...

RTS flow control doesn't seem to work

Posted on February 16, 2017 at 16:13Dear List,I am trying to get RTS/CTS flow control working on a discovery-stm32f407 board using cubemx generated software.But when sending data from the PC to the UART2 the RTS signal never gets high as seen with a...

Sietse by Associate III
  • 5728 Views
  • 7 replies
  • 0 kudos

can we use uart to communicate wire one wire device

Posted on June 15, 2017 at 08:08Hi all,I have DS18B20 sensor which works on the one wire protocol & it was interfaced to STM32F030C8T6 controller.But it was failed to communicate(respond) with the device over UART2.Below is the uart to device connec...

0690X00000603kHQAQ.jpg

I cannot find how to open stm32cube, package seems to have downloaded ok but no shortcut has appeared on the desktop

Posted on October 20, 2017 at 13:17Hi, I have downloaded stm32cubef4 for the nucleo-64 board (stm32f401). The directory seems to have the correct structure. No icon has appeared on the desktop or in the launch menu (win10) to start the program. Anyo...

STM32F7 SPI DMA triggered by EXTI

Posted on October 20, 2017 at 14:50Hi AllI'm looking for solution. I have to communicate my external ADC with STM32F7 by SPI. I have request from ADC on DRDY pin with 50kHz, which I set as EXTI in the procesor. But how to control SPI DMA by this DRD...

WakeUp Event detect from STANDBY mode

Posted on October 20, 2017 at 16:51I maked a little project with STM32F415, and i have 4 way to wakeup it from STANDBY mode.1) PA0 Pin wake up2) RTC Timer Wake Up3) Tamper1 Wake up4) RTC Alarm A and RTC Alarm BFor RTC Alarm i solved comparinging the...

Marco1 by Associate II
  • 1557 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L4 timers synchronizing

Posted on October 15, 2017 at 23:57Hello engineers,iam worikn on one project and i want to sync timers. Please correct me if iam wrong but in block diagram is shown ITR as control signal for whole timer(so all channels ale controlled by one ITR sign...

marek2399 by Associate II
  • 2914 Views
  • 6 replies
  • 0 kudos

STM32F429 DISC1 & keil5 & Embedded_Wizard

Posted on October 20, 2017 at 13:38i currently using ''keil5'' and ''STM32F429-DISC1'' and ''Embedded_Wizard''i happend some problem.that is keil software packi currently using editional version of ''Embedded Wizard''my problem is that required Keil...

0690X00000608ciQAA.png 0690X00000608jhQAA.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.