STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 SPI DMA Unexpected Overrun Error

Posted on October 17, 2017 at 01:30Hi everyone!I'm working with an external IC which must be read with a 'burst transfer'.I have to receive 122 half words (16 bit spi transfers), so I use an SPI DMA reception.When I configure a buffer in my code as ...

RTC cause main code stop working

Posted on October 21, 2017 at 01:06I was running RTC with stm32f051. I use cmsis and using LSE(32.768 khz) for rtc.I use this code for setup rtc with alarm . when interrupt of rtc is running the other section of code stop working but the interrupt r...

STM32F4 DMA REQ and ACK for External DMA

Posted on October 21, 2017 at 02:13I'm trying to interface my STM32F407 MCU with a peripheral device that has independent DMA/MPU interfaces. The MPU interface is available in two modes (68 and 80) and the data bus width is available in 8-bit and 16...

Zaher by Senior II
  • 1660 Views
  • 2 replies
  • 0 kudos

Microcontroller as a Slave

Posted on May 19, 2015 at 09:41   I want to set up an EtherCAT Network, First I have installed IgH EtherCAT Master in my PC (Ubuntu 14.04) and RTAI 4.1 as RTOS Can I use microcontroller such as STM32 as a slaveThanks in advance

zeydrjeb by Associate
  • 2702 Views
  • 4 replies
  • 0 kudos

an4666 application note timers

Posted on October 21, 2017 at 18:33The original post was too long to process during our migration. Please click on the attachment to read the original post.

con3 by Senior
  • 946 Views
  • 0 replies
  • 0 kudos

USB OTG with STM32CubeF4

Posted on October 21, 2017 at 14:56Hi allI am using the STM32F429ZE microcontroller with STM32CubeF4 (V1.16.0) library. For my next project I need to switch between USB device and host mode. (Depends if a host/device is connected.)The hardware has a...

STM32L476 MSI + PLL

Posted on October 13, 2017 at 19:37What is the magic that PLL doesn't want to let go of MSI?I've been trying to switch MSI + PLL ON/OFF during STOP2 mode (to save battery), but the MSI + PLL hangs on for about 15 milliseconds. I'm first switching on...

Resolved! X-CUBE-AWS

Posted on October 20, 2017 at 04:17When I try to add the X-CUBE-AWS expansion library package to my STM32CubeMX (which has been updated to the latest version - 4.22.1) I get the error: 'This package version is not managed on this version of STM32Cub...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.