STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN -> How to send overload frame?

Posted on August 15, 2017 at 05:00Hi,has anyone ever managed to send a standard CAN overload frame on an stm32?So far, I could only find error handling for incoming frames but no way to send one myself.#can #overload

Can not connect to device

Posted on October 24, 2017 at 08:53Hi, I use ST-Link V2 eumlator and STM32 ST-Link Utility SW to flash STM32F103VE. At the beginning, it can flash for several days. Today it can connect to device(show device information), but can't flash. It show ca...

0690X000006049pQAA.jpg
kent gu by Associate III
  • 1816 Views
  • 4 replies
  • 0 kudos

Resolved! PWM shift or move question

Posted on October 25, 2017 at 13:08Dear all,I am programing a STM32F429 for creating 4 PWM for inverter aplication. I managed to create these 4 PWM using TIMER1 and channel 1, channel 2, channel 1 N and channel 2 N.The inverter works pretty good usi...

STM32F103 internal bootloader work on RS485?

Posted on October 25, 2017 at 16:32Hi,I am using STM32F103RET6 microcontroller. On my PCB, the USART1 channel is used as RS485 communication with a SN65HVD11HD transceiver.  That means to transmit/receive each character, the direction pins RE, DE pi...

Jian Chen by Associate II
  • 1327 Views
  • 1 replies
  • 0 kudos

STM32F373 design queries

Posted on October 24, 2017 at 16:00We are planning to use STM32F373RBT6 for the replacement of ATMEL XMEGA_128:I have the following queries related to the design as per my understandings: Is USB2.0 will support device mode only and will be used to ...

PK K by Associate
  • 2211 Views
  • 5 replies
  • 0 kudos

STM32F4 series pinout spreadsheet

Posted on October 25, 2017 at 04:58Does anyone know if there is an existing excel format version of pinout table, example: STM32F40xx pin and ball definition (Table 7 from STM32F4 series datasheet) available? https://community.st.com/tags♯/?tags=pin...

SRAM and DMA in STM32F7

Posted on October 23, 2017 at 14:00I am working on a project where I have a STM32F7 which shall read data from an external SRAM using DMA.The SRAM has 16 bit adressbus and 8 bit databus. I want the data to be copied to a 16bit buffer in the STM32F7 ...

rickard2 by Associate III
  • 5694 Views
  • 20 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.