STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't open the STVD software

Posted on October 25, 2017 at 11:04ST Visual DevelopHi All,I want to ask as i recently installed the STDV software in my new laptop window10 but i can't open it. Can please help me to solve this problem. Much appreciated for your kind help. Thanks.I...

0690X00000608fcQAA.png

DMA clock frequency

Posted on October 23, 2017 at 11:54Hello,Is it possible to change the DMA clock frequency ? If so, how to do that ?(STM32L071)

Rtc sync with Remote clock (Gps)

Posted on October 24, 2017 at 14:59Hi community,If any face this issue earlier, please help me out.I am working on stm32f417 board. Right now Am trying to sync rtc time with gps timing, but Am seeing drift in subseconds field of rtc.Am programming t...

Problem stm32cube_fw_l4_v190.zip

Posted on October 24, 2017 at 08:44HelloInstalled STM32CubeMX-4.22.1. I create the first project (on STM32L452CE) and I can not download from the site stm32cube_fw_l4_v190.zip. Can tell me where to download stm32cube_fw_l4_v180.zip?@

STM32F103RET6 bootloader question

Posted on October 24, 2017 at 22:05From AN2606, to make STM32F103RET6 going into the bootloader mode, I need to pie BOOT0 pin to VDD and BOOT1 pin to GND.  Is there way I can make the chip go into bootloader mode with BOOT0 pin tied to ground?  I am...

Jian Chen by Associate II
  • 1325 Views
  • 1 replies
  • 0 kudos

Resolved! Why is there no output from TIM9 CH2 on PE6

Posted on October 24, 2017 at 01:21I am using the STM32F429ZI.  I have setup four timers to slave from TIM3.  The timers are TM1, TM2, TM4, TM9.  All four are setup the same as PWM generators in One Pulse Mode and I have checked multiple times to ma...

RTC usage on F1 serie

Posted on October 23, 2017 at 16:55Hi there,I started the RTC implementation on my STM32F103 with Cube.This is the initialisation code developed by Cube:static void MX_RTC_Init(void){RTC_TimeTypeDef sTime; RTC_DateTypeDef DateToUpdate;/**Initialize ...

Fede Rico by Associate III
  • 1464 Views
  • 3 replies
  • 0 kudos

STM32CubeMx autogeneration bug with C++ ?

Posted on October 19, 2017 at 19:01HelloCubeMX 4.22.1Cube for L1 1.8CubeMx generates this kind of code in every initialization file like, for example 'adc.h'#ifndef __adc_H#define __adc_H#ifdef __cplusplusextern 'C' {#endif< snip>extern void _Error_...

JulienD by Senior
  • 842 Views
  • 1 replies
  • 0 kudos

SD-Card problem (X-NUCLEO-IDW04A1)

Posted on October 24, 2017 at 15:03Hello!I'm using the X-NUCLEO-IDW04A1 evaluation board. The problem is that I can't communicate with the SD card. I've tried the following AT commands 'AT+S.FSC=test.txt, 1000', 'AT+S.FSC=0:test.txt, 1000' and 'AT+S...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.