STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST, don't use /** **/ for one line comments

Posted on October 26, 2017 at 22:43 Because IDE does not like nested comments. I am commenting several lines of example code but some idiot has put every other line an one line a /* */ comment. Fix that software please. Not like this: /...

LMI2 by Lead
  • 3297 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F303 Nucleo-144: which IDE to use for Development?

Posted on April 06, 2017 at 13:36Hi,I have a STM32F303 Nucleo-144 Development Kit and struggling to figure out which IDE to use. This is first project with Cortex-M micro-controller and I have a few queries:* If somebody who is aware of the software...

Prasant J by Associate III
  • 2608 Views
  • 5 replies
  • 0 kudos

Resolved! CY62177EV30 SRAM with STM32L496AEI

Posted on October 19, 2017 at 09:53Greetings people,I was wondering if the SRAM by CY62177EV30  is compatible with the FMC on STM32L496AEI with 20 bit address width and 16 bit data width.I can only use 20 bits from the address bus because of pin mul...

Boot from SRAM

Posted on October 23, 2017 at 10:49I have a question about the stm32f103xx. I want to know how it boots from Embeded SRAM. I have known that the IBUS of Cortex-M3 can't access the SRAM from the reference manual. When boots from the SRAM,  how Cortex...

l yk by Associate II
  • 6453 Views
  • 14 replies
  • 0 kudos

Disable STM32F103 Independant Watchdog

Posted on October 19, 2015 at 11:01Hello,In one of our projects we have implemented IWDG (independant watchdog). There is a condition in the software that when the power supply fails, the controller STM32F103(Powered By Rechargeable Battery) puts it...

gada by Associate III
  • 4099 Views
  • 4 replies
  • 0 kudos

nucleo board communicate with raspberry pi through SPI

Posted on October 27, 2017 at 14:57the task is to make nucleo board L476 to commucate with raspberry pi 3 through SPI. Now the code on both sides are finished and build successful. But I don't know how to test if the data are sent successfully. Is t...

Shared memory between BL and Main application

Posted on October 19, 2017 at 10:46 I am working on the project with STM32F030R8T6. So far I have bootloader and main application with memory space allocated. My problem is that currently I am jumping between main and bootleader using address of re...

Resolved! CubeMX USB_DEVICE middleware problem on V1.9.0

Posted on October 27, 2017 at 13:25Hi, I just moved a code from a STM32L476RCT6 on cubeMX V1.7.0 to V1.9.0I didn't change anythingWhen I start the push and start the program, it crash on the SystemClock_Config() with the new version. I tried again w...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.