2017-10-26 1:43 PM
Because IDE does not like nested comments. I am commenting several lines of example code but some idiot has put every other line an one line a /* */ comment.
Fix that software please.
Not like this:
/* Insert a delay of display */
HAL_Delay(2);
}
/* Clear the Background Layer */
BSP_LCD_Clear(LCD_COLOR_BLACK);�?�?�?�?�?�?
//
2017-10-26 9:55 PM
Maybe call this a MISRA consequence more than ST's for compatibility with all users out there
(for industrial or automotive, sometime the tools are kept the same for 10 years without upgrades)
https://stackoverflow.com/questions/9538589/rationale-for-comment-rules-in-misra
My workaround for this is
#if 0
junked source code
#endif
2017-10-27 12:11 AM
/ * Used for compatibility with dinosaurs from 1998 * /
Modern IDs often get malfunctioned in the code syntax highlighting module - due to stack overflow. There is a technical limit of 65k lines - below which the plug-in begins to suffer from amnesia. When the amnesia boundary falls / * neatly between several lines of comments * / - the synchronization is violated and the user sees a frank porridge. For example, the incorrect operation of conditional operators #if.Everything was fine while the projects were thin.Using // for comment, and /// for an important comment - solves the problem of amnesia.2017-10-27 8:59 AM
,
,
Interesting
I wonder why Keil Ide is so upset of this when this problem has been there for years.
I have to try this
♯ if 0
junked source code
♯ endif
Using // for comment, and /// for an important comment - solves the problem of amnesia.
Yes but when the one with dementia is ST, what can you do.
LM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.