STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to synchronize DAC, ADC together?

Posted on October 31, 2017 at 07:13I am using stm32L476 discovery board. I am trying to generate triangular wave with DAC. I am using two lookup tables for the DAC(1 for each up slope and down slope). I am giving sine wave at ADC input and I am gett...

C S by Associate II
  • 2364 Views
  • 2 replies
  • 0 kudos

stm32f373 adc ftrig

Posted on October 30, 2017 at 05:13Hi,Looking at the other stm32 MCU's like the stm32f407 I see in their datasheet a spec fTRIG (aka the External trigger frequency) ... however I cannot see the same spec for the 16bit SDADC on the stm32f373 datashee...

othane by Associate II
  • 1747 Views
  • 3 replies
  • 0 kudos

STM32F3Discovery Project in Ac6/OpenSTM32

Posted on October 31, 2017 at 23:30Hi forum,I have downloaded the STM32F3Discovery Demo Source Project.There are project files for several IDEs included but looks like none for Ac6/OpenSTM32.Has somebody converted that already?

STM32CubeMX project reuse

Posted on September 26, 2017 at 17:56If I have .ioc project for a UFBGA176 and then I want to migrate to an LQFP144, is there a way to proceed with STM32CubeMX without loosing all the work in 'Configuration' tab?In other words is there a way to sepa...

LRWAN_V1.1.1 example PA0 and PA4

Posted on October 30, 2017 at 10:26Hi,I am using the B-L072Z-LRWAN1 board running the End-Node example.I added 4 GPIO external interrupts on PA0,PA2,PA3 and PA4.Before the the board goes into Stop Mode all 4 intterupts works as expected.//----PA0, P...

how can i use LCD 4*20 in IAR with CMSIS?

Posted on October 30, 2017 at 09:18hi.i want to use LCD 4*20 in IAR with CMSIS  , but i didn't found any library for this.and if i dont want to write a library for lcd , what do i do ?where do i can found this library?or shall i write this library?o...

tim3 rises all interrupt flags even though it shouldn't

Posted on October 31, 2017 at 11:46Hello, I have timer 3 setup like this:ARR = 8400PSC = 99CCR1 = 4200CCR2-4 = 0xFFFFCR1.CEN = 1DIER.CC1IE = 1DIER.UIE = 1when i run my code after one interrupt all interrupt flags get set to 1, obviously this shouldn...

stm32f401rc encoderMode of tim9 do not work

Posted on October 31, 2017 at 11:27I used the PA2 PA3,the TIM9->CNT do not changevoid MotorBEncoder_Init(void){ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_ICInitTypeDef TIM_ICInitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2Per...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.