2017-10-31 3:27 AM
I used the PA2 PA3,the TIM9->CNT do not change
void MotorBEncoder_Init(void)
{ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_ICInitTypeDef TIM_ICInitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM9, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_OD; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure);GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_TIM9);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_TIM9);TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
TIM_TimeBaseStructure.TIM_Prescaler = 0x0; TIM_TimeBaseStructure.TIM_Period = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM9, &TIM_TimeBaseStructure); TIM_EncoderInterfaceConfig(TIM9, TIM_EncoderMode_TI12, TIM_ICPolarity_Rising, TIM_ICPolarity_Rising); TIM_ICStructInit(&TIM_ICInitStructure); TIM_ICInitStructure.TIM_ICFilter = 5; TIM_ICInit(TIM9, &TIM_ICInitStructure); TIM_SetCounter(TIM9,0); TIM_Cmd(TIM9, ENABLE); }2017-10-31 3:49 AM
TIM_TimeBaseStructure.TIM_Period = 0;
Set it to nonzero - best to 0xFFFF.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.