STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Receiving duplicate bytes in DMA output

Posted on October 31, 2017 at 21:32 My project involves sending packets of bytes out of the serial port using DMA. I am using an STM32F417 with DMA2 using USART3. DMA transmit buffer is set to The packets that stream the current head position (liv...

Looking for simple low-level code to toggle a pin

Posted on November 01, 2017 at 16:01I'm not having any success in simply toggling a pin on a STM32F303 Nucleo-32 evaluation board. I'm using Keil uVision V5.24.2.0. Also I'm trying to do this at a level below the HAL interface. With the community's ...

stm32h7 pin configuration tool

Posted on October 31, 2017 at 13:53I'm a circuit board designer and I've been given a set of requirements to map a given set of functions out of the STM32H7.  Is there a pin configuration tool that allows a user to specify which functions (CAN, ULPI...

Nucleo F767ZI + lwIP+ Cube MX issues

Posted on September 29, 2017 at 16:45 Hi all, i'm a new nucleo user and I start to play with the F767ZI. I will usethe nucleo for send periodical http get request to a remote server, but till now i have some issues with the tools. I configure cub...

Di Ci by Associate II
  • 8939 Views
  • 19 replies
  • 0 kudos

What would be the best practice to disable an interrupt?

Posted on November 01, 2017 at 11:42Hi,In your opinion, what would be the proper way to disable an interrupt, disabling only the peripheral enable bit or also the NVIC bit?Is there a risk to disable only the peripheral bit and leaving the NVIC IRQ e...

stm32f2 MCO switching off

Posted on November 01, 2017 at 09:33Hi,I am migrating from stm32f103 to stm32f205.stm32f103 allows switching MCO on by HAL_RCC_MCOConfig(RCC_MCO, RCC_MCO1SOURCE_HSE, RCC_MCODIV_1) and off MCO by HAL_RCC_MCOConfig(RCC_MCO, RCC_MCO1SOURCE_NOCLOCK, RCC...

Boris Hoz by Associate II
  • 1723 Views
  • 2 replies
  • 0 kudos

STM32CubeMX Project rtos+lwip STM32F746ZGYx

Posted on November 01, 2017 at 13:30IDE :Eclipce OpenSTM32: ac6    after compiling the project  i get  this error #ifndef LWIP_TIMEVAL_PRIVATE#define LWIP_TIMEVAL_PRIVATE 1  #endif#if LWIP_TIMEVAL_PRIVATEstruct timeval { long tv_sec; /* seconds */ l...

stm32f103ret6 flash erase problem

Posted on October 31, 2017 at 16:22Hi,I need to perform STM32F103RET6 flash memory operation: erase, write.  My erase failed.  Anybody has the EWARM project for internal bootloader(burnt to chip from factory)?  Or any working flash routines for STM3...

Jian Chen by Associate II
  • 1989 Views
  • 3 replies
  • 0 kudos

Hi, i want drivers for stm32l476mcu

Posted on November 01, 2017 at 10:38Hi,I bought stm32l476 micro controller. I want drivers for this board(stm32l476).please send me the link where i can get those drivers.Regards,Ashok

stm32f205 USB and new project questions.

Posted on November 01, 2017 at 08:48Good morningStm32F205RBT We are planning a new project to control with MCU.I'll use the LCD,Use the six buttons (Enter, esc, left, right, up, down) to set the timeEach IO will be recorded in the flash ROM when the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.