2017-11-01 8:01 AM
I'm not having any success in simply toggling a pin on a STM32F303 Nucleo-32 evaluation board. I'm using Keil uVision V5.24.2.0. Also I'm trying to do this at a level below the HAL interface. With the community's help I am able to do an simple ADC->DAC project that runs off the HSI as the system clock. Then I tried to toggle a pin to monitor the sampling rate with no luck. To learn about GPIO digital output pins I have created the simple project below. I'm looking for someone experience with the lower level programming to take a look and hopefully find my problem. Using my ADC->DAC program AND the data sheet, the STM32F303K8 part comes up with the clock defaulted to HSI so a clock setup for my test should not be needed (???). As seen, after the brief setup I'm trying various methods to toggle PA0 but with no success. Any ideas? What am I missing? Thanks... Randy
#include <stdint.h>
#define BIT0 (1 << 0)#define BIT1 (1 << 1)#define BIT16 (1 << 16)#define BIT17 (1 << 17)#define REGISTER_32(ADDRESS) (*((volatile uint32_t *)(ADDRESS)))
#define REGISTER_16(ADDRESS) (*((volatile uint16_t *)(ADDRESS)))#define REGISTER_8(ADDRESS) (*((volatile uint8_t *)(ADDRESS)))#define GPIOA_BASE 0x48000000
#define GPIOA_MODER REGISTER_32(GPIOA_BASE + 0)#define PERIPH_BASE ((uint32_t)0x40000000)
#define AHB1PERIPH_BASE (PERIPH_BASE + 0x00020000)#define RCC_BASE (AHB1PERIPH_BASE + 0x00001000)#define RCC_AHBENR REGISTER_32(RCC_BASE + 0x14)#define GPIOA_ODR REGISTER_32(GPIOA_BASE + 0x14)
#define GPIOA_BSRR REGISTER_32(GPIOA_BASE + 0x18)#define GPIOA_BRR REGISTER_32(GPIOA_BASE + 0x28)int main(){ GPIOA_MODER |= BIT0; //set PA0 to digital. other setting default GPIOA_MODER &= ~BIT1; RCC_AHBENR |= BIT17; //Enable portA clock while(1) { GPIOA_ODR |= BIT0; //set GPIOA_ODR &= ~BIT0; //reset GPIOA_BSRR |= BIT0; //set GPIOA_BRR |= BIT0; //reset GPIOA_BSRR |= BIT16; //another type reset } return 0;}2017-11-01 8:23 AM
Probably want to enable the clock *before* you program synchronous registers...
Keil has a peripheral viewer, you should perhaps use that as you step your code.
>>
I'm looking for someone experience with the lower level programming to take a look and hopefully find my problem.
8th RULE:
If this is your first night at FIGHT CLUB, you HAVE to fight.2017-11-01 9:56 AM
Great catch!
The below change allows the pin to toggle.
RCC_AHBENR |= BIT17; //Enable portA clock
GPIOA_MODER |= BIT0; //set PA0 to digital. other setting default
GPIOA_MODER &= ~BIT1;
Thanks! Is the ordering of setting registers defined somewhere or is this just experience?
I'm looking through the RM0316 'STM32F303xB/C/D/E, STM32F303x6/8, STM32F328x8, STM32F358xC, STM32F398xE advanced ARM®-based MCUs' and cannot find a suggested ordering of register setups for GPIO pins.
Also any idea why these lines will toggle the pin:
GPIOA_ODR |= BIT0; //set
GPIOA_ODR &= ~BIT0; //reset
but these lines do not:
GPIOA_BSRR |= BIT0; //set
GPIOA_BRR |= BIT0; //reset
GPIOA_BSRR |= BIT16; //another type reset
Thanks...
Randy
2017-11-01 11:58 AM
Found in RM0316 where 'Before using a peripheral user has to enable its clock in the RCC_AHBENR, RCC_APB2ENR or RCC_APB1ENR register.'
Now to better understand the GPIOx_BSRR and GPIOx_BSR.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.