STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

OpenOCD support for external STLink debugger

Posted on November 05, 2017 at 07:41Hi all,Is anyone using OpenOCD with genuine external STLinkV2 debugger/programmer and STM32L0? Clearly, there is an issue as I have tested multiple units and OpenOCD releases (0.9, 0.10.).The debuggers are fully f...

How to use HAL SPI Library

Posted on November 08, 2017 at 16:02Is it possible to use the HAL slave SPI library to receive an unknown number bytes from the master? I'm convinced I'm missing something since the packet size is rarely known in the projects I work on but for some ...

Konami by Senior II
  • 2079 Views
  • 5 replies
  • 0 kudos

STM32F7 HAL I2C Reading bytes out of sync

Posted on April 25, 2016 at 15:27We're currently talking to a few I2C devices on the same bus using latest STM32F7 HAL drivers.All works fine for a while (minutes or hours) and the bus debug on our scope looks perfect, however, every so often we hav...

AndyJT by Associate III
  • 2454 Views
  • 4 replies
  • 0 kudos

Resolved! Understanding SysTick_Handler()

Posted on August 28, 2017 at 13:46Hello everyone,I am setting up a project to make some tests with an STM32F7 MCU. I am using the STM32Cube HAL and the idea is to configure some timers and their interrupts using this HAL. The board is equipped with ...

Quick start STM32F7

Posted on November 14, 2017 at 16:491. I have necessity force to start STM32F7 after reset as fast as possible.How to do it correctly using HAL or Low-layer drivers?In 'Description of STM32F7 HAL and Low-layer drivers' I find in chapter 'FAQs'Follow...

creating bootloader for sensor tile

Posted on September 29, 2017 at 21:33I am using the ST SensorTile for development.  Now trying to understand the OTA and Bootloader.Currently only able to find the binary for bootloader.Does ST provide source code / project to build our own bootload...

Resolved! Please Correct BUG with SD code generation

Posted on March 02, 2017 at 18:57The new format of code generation makes a BUG in the file: bsp_driver_sd.hThe BUG prevent building FAT_FS modulesTo solve the issue line 67 should be changed with the following ones:&sharpifndef BSP_SD_CardInfo  &sha...

Have you come across UNI/O source code for STM32?

Posted on July 01, 2015 at 15:48I am working with the STM32F407 microcontroller and I need to interface to a one-wire serial flash memory from Microchip using their UNI/O protocol (https://en.wikipedia.org/wiki/UNI/O). I am new to ST microcontroller...

arnold_w by Senior II
  • 1378 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.