Resolved! AN4879 does not list STM32C5 as applicable products
Newest AN4879 does not list STM32C5 as applicable products.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Newest AN4879 does not list STM32C5 as applicable products.
Hi everyone, I am trying to setup DCMIPP Pipe0 to read data from 256x192 pixel sensor by 16 data lines. Seems everything configured and working fine except of transfer data to destination buffer. DCMIPP frame counter is increasing. Pipe0 dump counte...
Hi Team, I am designing a custom PCB using STM32H753 and planning to use the QUADSPI peripheral for external memory. My use case is data read/write (indirect mode) — not XIP or memory-mapped execution. While working in STM32CubeMX, I came across some...
Hi,I am working with the STM32N6 series MCU on the STM32N6570-DK board and have encountered a pin multiplexing conflict.As per the schematics and datasheet:PA15 (JTDI) and PB4 (JNRST) are multiplexed with LTDC signalsThese pins do not appear to have ...
Hello ST,What is the maximum current draw into the STM32H563/573's VDDUSB pin, please? Is this the same as IDD(USBBCD), i.e. 300 uA (ds14258 rev.6 Table 120)?
STM32L052TIM21, Channel 1: Output PWMTIM21, Channel 2: Switching between Output PWM and Input CompareSystem Clock: 32 MHzHello,I want to use TIM21 of STM32L052 for PWM output on channel 1 and input capture on channel 2 simultaneously. uint16_t TIM_CC...
The development board I am using is stm32h723. Assuming I only configured region 0 and wrote a blacklist, all regions (both privileged and non-privileged) are inaccessible. The remaining 15 regions were not configured. However, in the MPU Control Mod...
①Fault Phenomenon: The fourth physical output core acquisition pin is faulty. Without any external connections, the voltage at the CPU pin measures around 4.3V, whereas it should normally be 0V. This also causes the operational amplifier chips connec...
Could you please tell me how many CAN interfaces are there in STM32H723? I asked the AI, and the AI said there are 2. But when I configured it using Cubemx, I found there are 3. Help me, please!
I'm trying to use the internal CRC calculation unit in the STM32H7 FLASH controller via the HAL_FLASHEx_ComputeCRC() api. I've finally started getting crc32 values returned but can't match them against any common algorithms ... reviewing AN5507 impli...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.