STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Changes required in the CAN configurations for stm32f413xx, since the below configurations in the code is not working

Posted on December 08, 2017 at 12:32void MXCAN1Init(void){    __HAL_RCC_CAN1_CLK_ENABLE();    stat_stCAN_HandleTypeDefHCan1.Instance = CAN1;    //stat_stCAN_HandleTypeDefHCan1.Init.Prescaler = (U16)((U32)HAL_RCC_GetPCLK1Freq() /    //               ...

Trigger SPI DMA by EXTI

Posted on December 14, 2017 at 14:10Hi there,I' m programming an STM32L496 and want to read samples from an external ADC (ADS1292R) using SPI with DMA.Each time the ADC has a new sample ready, it drives the DRDY line low. Currently, I use the EXTI I...

0690X000006093nQAA.png
braucadr by Associate
  • 1888 Views
  • 0 replies
  • 0 kudos

STM32L072 vs STM32L082 detection

Posted on December 13, 2017 at 22:11This one sounds simple. Essentially STM32L082 has a AES peripheral over STM32L072. I simply want to have a way to find out whether it's there or not.Now RCC->AHBENR does not help. I can set the corresponding bit ....

STM32F405 UART CTS RTS flow control issue

Posted on December 14, 2017 at 13:50Hello,We are using STM32F405 controller with CUBE MX library for UART communication with hardware flow control. Our aim is to wakeUp STM board from STOP mode when UART data comes. So I monitor RTS and CTS lines an...

Resolved! MCU Selection for a communication moduel

Posted on December 11, 2017 at 11:40Hi All,We have a requirement with the following communication interfaces: Local RS232 communicationRJ45 for remote communication (Ethernet SNMP Interface)RJ114 line displayThis communication MCU shall be interfac...

Timer adapted to HAL Standards from previous code

Posted on December 14, 2017 at 12:42Hi,I'm trying to adapt the following code, from previous versions, to HAL Cubemx standards :void TIM1_CC_IRQHandler(void){uint32_t break_time, mab_time;TIM_ClearITPendingBit(TIM1, TIM_IT_CC1);break_time = TIM_GetC...

ignasi by Associate II
  • 779 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.