STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use SD card memory as Extended RAM

Posted on January 23, 2018 at 13:24Hi STM community, Currently we are developing an application with STM32F779I eval board.I am using Cube Mx and System work bench for STM32. We are facing issue with RAM.My application uses FreeRTOS, FatFS and SD Ca...

Problem with stm32F446 output on pa6 and pa7

Posted on January 22, 2018 at 21:58Hi, I've made a pcb using the stm32F446 mcu, 64 pin package, but I have a problem with it. I have four LED's attached to pa4 to pa7. Two of these work fine, but the ones on pa6 and pa7 only lights up entirely when ...

0690X00000603qmQAA.jpg

DS18B20 HAL lib for STM32F0

Posted on January 23, 2018 at 14:33Hello,I have been looking for a library for the ds18b20 compatible with stm32f0 and with the HAL driver but without success, so I decided to modify old one to make it compatible.this lib uses while loop delay, the ...

RTC + STM32L NUCLEO + Contiki

Posted on January 23, 2018 at 10:37I found a strange behavior of the STM32L NUCLEO cards. I installed a sensor network using Contiki and I implemented an RTC. If I try to set RTC_SYNCH_PREDIV to a value above 1023 (for example 2047, 4095, ... up to ...

simval986 by Associate II
  • 1131 Views
  • 1 replies
  • 0 kudos

stm32f407 -- PINRSTF is set after power cycle

Posted on January 23, 2018 at 14:43Should the NRST external reset (PINRST) be set on an STM32F407 after a power reset?I want to be able to count the number of each type of resets in my code. The problem that I have is that the NRST pin reset is alwa...

dibs by Associate II
  • 982 Views
  • 0 replies
  • 0 kudos

I2C comm issue between MCUs

Posted on January 23, 2018 at 12:57Hi,I am using I2C to send data between two STM32F4 MCUs with the same MCU working as a Master always. The master MCU controls a display and sends the slave a massage just when the user changes a parameter.I am usin...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.