STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK Utility for startup hardware tests of prototypes

Posted on January 26, 2018 at 08:42Want to use STM32 ST-LINK Utility for first hardware tests of prototypes with STM32F071 MCUs. E.g. switch LED on/off, set port pins, set dac values, read temp sensor of MCU and...and...As we want to use ST-LINK Uti...

JuM by Senior
  • 731 Views
  • 0 replies
  • 0 kudos

CubeMX became a cloud application

Posted on January 24, 2018 at 06:21So, the 4.24 version won't generate anything if it does not have an internet connection. Even if there is firmware in repository...Now I'm loving the earlier version with a passion! 

STM32F4XX SPI3 Data register is always 0xff and TXE is 1

Posted on January 22, 2018 at 19:55I am trying to interface SPI3 of STM32F4with external SPI F-RAm memory chip. But after writing dummy data(0x00) in data register, data register is set to 0xff and it doest not change and my TXE bit is always set. H...

Reema O by Associate II
  • 1194 Views
  • 5 replies
  • 0 kudos

STM32L162

Posted on January 24, 2018 at 20:29Hi,What is a start point for using STM32L162?

STM32L476 USB_OTG can't get recognized by Windows

Posted on January 25, 2018 at 21:23Version:1.0 StartHTML:0000000168 EndHTML:0000000993 StartFragment:0000000435 EndFragment:0000000976I have configured the USB_OTG as a mass storage on STM32L476VE that has a 8MHz external crystal, and when I connect...

CAN Controller TX does not show signs of life

Posted on January 24, 2018 at 03:15Can_TX is showing no activity. I can't figure out what I am doing wrong. I've set up the project with STMCubeMX to use CAN1 on PD0 and PD1. When I attempt to transmit there is no signs of life on the TX pin. Using ...

tyler2 by Associate II
  • 2328 Views
  • 4 replies
  • 0 kudos

Resolved! EXTI handler gets stuck

Posted on January 24, 2018 at 20:27 With my STM32F4 I am trying to use an external interrupt to read aquadrature encoder on PC02 and regular port PC The interrupt on PC02 fires when I move the encoder, but it won’t return to the main loop again a...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.