STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL & SPL coexistence

Posted on February 02, 2018 at 23:15Hello,I have a piece of code using STM32F103VE FSMC based on SPL and have some problem with porting it to HAL.It seems that the FSMC HAL structure is slightly different than the SPL - at least quick comparison doe...

Resolved! FDCAN STM32H743ZI-NUCLEO TX

Posted on February 02, 2018 at 12:34Hi all,I am trying to make a simple CAN test program to send 8 bytes data. It seems like it is sending data (from the code point of view) but when I look with a scope. The TX line goes down for a few �S, then go b...

ab val by Associate III
  • 3543 Views
  • 6 replies
  • 0 kudos

Resolved! IWDG (Watchdog) Enable on STM32

Posted on February 02, 2018 at 09:21Hi everybody,i'm tryng to configure the IWDG but it doesn't work. i didn't find the enable bit, is there?Can you help me?I post my code herevoid wdt_enable(void){ RCC -> CSR = RCC -> CSR | 0x00000001; //Enable LSI...

Resolved! Maybe error in CubeMX STM32F318C8

Posted on September 20, 2017 at 17:34Hello I find ''minor discrepancy'' between datasheet and CumeMX, alee last releas.In DS is NPOR pin on position 20 LQFP48 and in CubeMX in position 43.  and in DS is on 43 P7B and in CubeMX PB2 on 20 .

0690X00000608JAQAY.png
asrock70 by Associate II
  • 1528 Views
  • 2 replies
  • 0 kudos

STM32F437 IAP Option Byte programming failure

Posted on February 02, 2018 at 15:08So I have an STM32F437VG processor and I want to change the BOR level to 0 in the Option bytes (leaving all others at their factory defaults). I intend to do this via a one-time change in early startup via the fol...

andrew by Associate II
  • 822 Views
  • 0 replies
  • 0 kudos

Problem with ADC in STM32L476RGTx

Posted on February 02, 2018 at 09:45Currently I am working in an application using  STM32 controller.I am facing one issue.I am using 2 ADC's which are working for the first time right after flashing.     We use the independent MCU PCB(STM32-L476RGT...

How many Max Slaves in SPI

Posted on February 02, 2018 at 10:19In SPI protocol, how many  maximum slaves can I connect to master(nucleo STM32F103RB)?#stm32f103rb #spi-communication #nucleo-stm

STM32L4x2 Multimaster mode of UART

Posted on February 02, 2018 at 11:03Hi,is it possible to set the STM32L4x2 UART to a 9 bit address mode, where only the 9th bit create an interrupt or wake up from mute mode. Actually I see the only possibility to set only one address. But in some p...

josef2 by Associate II
  • 842 Views
  • 0 replies
  • 0 kudos

DMA transfer from DCMI to Flash or SD card?

Posted on January 24, 2018 at 19:50Hi My micro (STM32F765VI) has 512KB of SRAM. I have an OV7725 image sensor connected to it. I am right now performing a DMA transfer of RGB565 in 320x240 format from the image sensor to SRAM. This takes up 320x240x...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.