STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F030K6T6 can only be programed with ST-LINK once

Posted on February 03, 2015 at 08:40my design using STM32F030K6T6, see attached schematics, and using SWD to program, with ST-LINK(Version is at attached picture), I can only program STM32F030K6T6 one time, after code (which is simple toggle one LED...

Power Down Threshold in STM32L4

Posted on February 04, 2018 at 14:59Hi,I am using STM32L486 in my project.I have a question about the power-down threshold.What is the power down Threshold?The threshold that determin if it was BOR or power down reset.In power down reset the backup ...

Resolved! STM32 GPIOS mode.

Posted on February 03, 2018 at 18:07In STM32 there are two modes to configure GPIOS, input and output.In input mode we have,  Analog modeFloating InputInput with pull-up/pull-downIn output mode, General purpose output push-pullGeneral purpose outp...

Problem to set ADC Channell

Posted on February 03, 2018 at 16:11Hi all,i'm working with a STM32L053 processor and I'm having some trouble managing the ADC.My ADC is setup to work in discontinuous mode, so i set the channel to convert by using the following function:void system...

stm32f030cct6 / stm32f09xx family issue

Posted on February 01, 2018 at 11:50Hello,I am already using stm32f030c8t6 in various projects. And for larger flash controller i decided to opt for stm32f030cct6.when i read my target device having stm32f030cct6(printed on IC), it responds the mess...

How do I choose which development toolset to use?

Posted on February 01, 2018 at 17:40Just getting into STM32 programming and am bewildered by number of development tools, so many of which seem mutually exclusive.  Is there some sort of roadmap, guide to selection of tools?  Does STM32CubeProgramme...

Jack Juni by Associate II
  • 5337 Views
  • 11 replies
  • 0 kudos

Understanding STM32F0 GPIO Interruts

Posted on February 02, 2018 at 22:35Not sure if I understood the GPIO interrupt structure of the STM32F0 family correct.I can select either i.e. PA0 or PB0 as interrupt source but not both at the same time?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.