STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX and SysTick

Posted on February 02, 2018 at 16:09Why does CubeMX generate the following lines in SystemClock_Config if the HAL timer is set to anything other than SysTick?HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick */HAL_SYSTICK_CLKS...

adrian by Associate III
  • 6967 Views
  • 7 replies
  • 0 kudos

Resolved! STM32L031 alternate function

Posted on February 05, 2018 at 05:15I am using STM32L031 by power of battery, so I wish to save power consumption.Now the current consumption is about 200uA at stop mode.May I change SWDIO and SWCLK to analogue GPIO after initialization?May I furthe...

Auto update version

Posted on August 17, 2017 at 10:18Hello.      I am a test engineer in ABB of China. Now I need help .     My chip is  STM32F051R8T6 in our target.  After my company's R&D check in their codes, then build one version about the STM32F051R8T6 ,I need a...

HOW TO START WITH STM32F030K6T6?

Posted on February 04, 2018 at 05:06Hi,I am new to STM Controllers and i got project to work on STM32F030K6T6 Controller ,i don't know from where should i start. where can i get it's sample peripheral libraries,How does http://www.st.com/content/st_...

stm32f407 eeprom emulation

Posted on February 04, 2018 at 16:10Hello friendsI use STM32F4-Discovery stm32f407 eeprom emulation exampleBut the program will only run once after each DownloadFor the second time, jump to hard faultHow to solve this problem?Thanks

Pedram by Associate III
  • 2265 Views
  • 3 replies
  • 0 kudos

STM32F100RCT6TR TIM12 issues

Posted on January 06, 2016 at 18:39Hi!I am trying to control two motors using an STM32F100RCT6TR microcontroller and the standard peripheral library version 3.5.0. I want to use TIM3 channel 1&2 and TIM12 channel 1&2. TIM3 works perfectly but I get ...

Stm32f303 CDC problem

Posted on February 04, 2018 at 17:36Hello friends. I use STM32F303 discovery, and trying write code for usb cdc virtual com port, low level, registers only. 3 endpoints, 1st interrupt IN, 2nd bulk IN, 3th bulk OUT. I make it work, but have a problem...

Segger J link Debugging problem

Posted on February 04, 2018 at 16:05Hello,         I am using segger j link debugger if i download the Ac6 STM32 MCU GCC tool chain created project(current builder:Gnu Make builder) then code runs in debug mode,but if i download gitHub project then ...

0690X00000609bAQAQ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.