STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F769 Disovery ITM_SendChar

Posted on March 05, 2018 at 15:46Hi I am using Atollic studio and the STM32F769 Discovery board.I removed resistor R93 and fitted a 0R link to R92 so that the SWO line is connected to the ST-Link on the discovery board.I have followed this tutorial ...

Resolved! STM32F411VE Master-->SPI--> MAX7219 Slave

Posted on March 03, 2018 at 18:04 Hi, I beleive i have initialised my master STM32 correctly somehow i cant get my slave to understand my master. My problem is my slave does not seem to understand the master, i have tried various things, li...

0690X00000604RAQAY.jpg
tom.abel by Associate II
  • 3260 Views
  • 4 replies
  • 0 kudos

FSMC Controller (expand fpga and sdram)

Posted on March 06, 2018 at 03:41HelloI would like to expand the external memory using the STM32F429's FMC Controller.I want to connect BANK-1 to FPGA(like SRAM) and SDRAM bank(1 or 2) to SDRAM.Is it possible to use FPGA and SDRAM ?- sdram interface...

0690X00000609wIQAQ.png 0690X00000609wNQAQ.png

Must GPIO register be configured for trace port

Posted on April 22, 2015 at 14:15Hi, I'm working with the STM32F107. I would like to use the TPIU (trace port interface unit) with my uLinkPro. Do I have to configure the GPIO registers? I already set the DBGMCU_CR register. Thanks Matt

About STM32F4-Discovery USB Mass Storge

Posted on March 06, 2018 at 02:22Hi All    I test the USB Mass Storage in my STM32F4-Discovery when I plug to my PC through MircoUSB connector(CN5). My PC tell me ''USB Mass Storage Device Driver Error'', I don't know what's wrong?  Have any referen...

0690X00000609tKQAQ.png 0690X00000609HsQAI.png 0690X00000609wSQAQ.png 0690X00000609tfQAA.png

STM32 CUBEMX SYS Debug Settings

Posted on March 04, 2018 at 07:11 Here is the SYS debug settings Here is what CubeMX did. My questions is: I use Serial Wire and Trace Synchro Sw (4 bits) most. Here is the SYS debug settings Here is what CubeMX did. My questions is: Here ...

0690X00000609uHQAQ.png 0690X00000609oyQAA.png 0690X00000609ozQAA.png

SD card using SPI initialization stm32f303 issue

Posted on November 30, 2016 at 16:21 Hello, I am sending the correct command and I can see it on the scope.However, I don't get 0x01 response(I keep getting 0xff) from SDcard(SDHC)(SanDisk Ultra 40MB/s ...16GB) I am using the following code:uint8_t...

alkuor by Associate II
  • 2517 Views
  • 2 replies
  • 0 kudos

How to interpolate and compare 2 sine waves

Posted on February 28, 2018 at 22:23 Hi everyone, With my STM32F103C8T6 I would like to receive the 2 signals I1 and I2 from the picture below in order to convert to https://community.st.com/tags#/?tags=square%20signal. All the square part is...

0690X00000609qZQAQ.png
paul sauv by Associate III
  • 12242 Views
  • 19 replies
  • 0 kudos

Resolved! STM32L496ZG Nucleo-144 CAN initialization

Posted on March 05, 2018 at 15:19 I have Nucleo-144 Board with a STM32L496ZG and use it for evaluation if the MCU will work for us. But I´m stuck with the CAN initialization. I have the following init code: // CAN clock LL_APB1_GRP1_EnableC...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.