STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WizNet W5300 DHCP

Posted on January 17, 2017 at 09:16Hello,I am working on project where i need to interface STM32F429 to W5300. This is done with FMC SRAM interface. I tested that i have working hardware by reading chip ID, and id did returned 0x5300.Question is how...

STM32L0xx UART overrun error

Posted on March 07, 2018 at 13:04We are using the STM32L0 HAL implementation of the UART driver. The UART (115200,8-N-1) is used in interrupt mode and we have configured the interrupt to occur for every character. This is done so that we can impleme...

How do I make my own musical instrument?

Posted on March 04, 2018 at 18:46I plan on making a compact version of a musical instrument called Mridangam (an Indian musical instrument). The original instrument is pretty huge and there are different variants of it to produce different kinds of ...

STM Studio - only Array variables visible for F4?

Posted on February 15, 2017 at 06:52Hi,I am having a problem using STM Studio (version 3.5.1) - variables that are not arrays are not available to be imported and traced, while arrays are available. The problem is specific to the F4,  I have verifie...

stm32l476 External interrupt

Posted on March 07, 2018 at 09:15Hi,I am trying to use external interrupt.  I connect the PB3 to external output and I want to detect ricing voltage.I Using microcontroller STM32L476RG on Nucleo-L476RG.Moreover,I found the example that explained how...

Boris Fi by Associate
  • 2037 Views
  • 2 replies
  • 0 kudos

UART data transmit DMA problems

Posted on March 06, 2018 at 16:22Hello,i am working on a application where i try to measure a motor speed and current,  and then send the data to the PC using serial uart.The device used is a STM32F427For controlling the motor i used a timer1 6pwm c...

0690X00000609xBQAQ.png
Bogdan by Senior
  • 2077 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.