STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SD card access through MSC

Posted on November 24, 2017 at 22:21Hello,I am trying to make a MSC USB device to access SD card files.The computer recognizes the mass storage device, but cannot open the folder. After a while, it says the device was unrecognized.My code from usbd_...

Resolved! STM32F1 - LL_GPIO_Init() problem

Posted on March 17, 2018 at 20:45 Hi, A piece of code from STM32CubeMX v4.0 and latest F1 drivers generated for STM32VLDiscovery (the button is pulled-down by external resistor): static void MX_GPIO_Init(void) { LL_GPIO_InitTypeDef GPIO_Ini...

0690X0000060A77QAE.png 0690X0000060A9WQAU.png

Nanosecond delay

Posted on March 18, 2018 at 15:32 EDIT: Not sure where my intro paragraph went on the first time I posted. I have the below code working with inline assembly nops. Now I want to have the code be clock independent. The below code is my attempt ...

joe23 by Associate II
  • 4582 Views
  • 9 replies
  • 0 kudos

STM32CUBE MX and KEIL5 IDE

Posted on March 18, 2018 at 08:30Hi, I have been using STM32CUBEMX ide for building the code with Keil5 IDE. The issue or bug is the code is working fine when I am placing my code in the main function. But, when I create my own file or outside the m...

Kumar B by Associate II
  • 4489 Views
  • 15 replies
  • 0 kudos

STM32L4 low RTC precision

Posted on March 05, 2018 at 07:57 Hello there, I am using an STM32L4 family MCU. In an application, the RTC peripheral is utilized and clocked from an external crystal: The problem I have noticed just now is that with time, the RTC timer ...

0690X00000609xVQAQ.png 0690X00000609vUQAQ.png

unusual power consumption by stm32l152cb in run mode

Posted on August 14, 2014 at 14:22I am running a sample code with while(1) loop running from flash using MSI @ 2Mhz  and it takes 6mA, but the data sheet shows that it takes 1mA with MSI @ 4.2Mhz running from flash.Are there any other configurations...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.